Skip to main content
ASimo.3
Associate II
January 13, 2023
Solved

STM32U5 ADC hangs at calibration

  • January 13, 2023
  • 2 replies
  • 3700 views

I have a nucleo-U575ZI-Q and can run the examples for the ADCs just fine. However when I try and make my own project using STM32CubeMX the code hangs at the ADC calibration. I've gone over the settings a dozen times and compared them against the example and cannot find anything different. Any insight would be helpful. Thanks

This topic has been closed for replies.
Best answer by ASimo.3

Ok I figure it out. But this really should be noted somewhere in the examples. This line needs run before the ADC usage. HAL_PWREx_EnableVddA(); Im sure there are other ways to setup the Voltage reference, but in the simplest case this works. In the example projects it is buried in stm32u5xx_hal_msp.c here:

void HAL_MspInit(void)
{
 /* USER CODE BEGIN MspInit 0 */
 
 /* USER CODE END MspInit 0 */
 
 __HAL_RCC_PWR_CLK_ENABLE();
 
 /* System interrupt init*/
 
 /* USER CODE BEGIN MspInit 1 */
 HAL_PWREx_EnableVddA();
 HAL_PWREx_EnableVddIO2();
 /* USER CODE END MspInit 1 */
}

CubeMX doesnt seem to generate this, it looks like whoever made the example stashed those lines there.

2 replies

ASimo.3
ASimo.3AuthorBest answer
Associate II
January 13, 2023

Ok I figure it out. But this really should be noted somewhere in the examples. This line needs run before the ADC usage. HAL_PWREx_EnableVddA(); Im sure there are other ways to setup the Voltage reference, but in the simplest case this works. In the example projects it is buried in stm32u5xx_hal_msp.c here:

void HAL_MspInit(void)
{
 /* USER CODE BEGIN MspInit 0 */
 
 /* USER CODE END MspInit 0 */
 
 __HAL_RCC_PWR_CLK_ENABLE();
 
 /* System interrupt init*/
 
 /* USER CODE BEGIN MspInit 1 */
 HAL_PWREx_EnableVddA();
 HAL_PWREx_EnableVddIO2();
 /* USER CODE END MspInit 1 */
}

CubeMX doesnt seem to generate this, it looks like whoever made the example stashed those lines there.

Amel NASRI
ST Technical Moderator
January 19, 2023

Hi @ASimo.3​ ,

The sequence to be applied in order to enable analog peripherals is described in page 371 of RM0456 (paragraph: Peripheral voltage monitoring (PVM)).

So, in your case, only HAL_PWREx_EnableVddA() is required unless you need to use one of the pins GPIOG[15:2].

I confirm that this needs to be generated by STM32CubeMX, so thanks for bringing this issue to our attention. I reported issue internally.

Internal ticket number: 143303 (This is an internal tracking number and is not accessible or usable by customers).

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.