2019-12-09 3:19 AM
EDIT: Nevermind this thread can be deleted, apologies. I didn't enable the HSEM2 Global interrupts under NVIC1/2 in CubeMX.
Hi,
I'm having issues getting the hardware semaphore interrupts to function correctly, or I'm misunderstanding their usage. I'm using a cubeMX generated project in SW4STM32. Below is a code snippet from the main.c file on the M4.
uint32_t sem_mask = __HAL_HSEM_SEMID_TO_MASK(8);
HAL_HSEM_ActivateNotification(sem_mask);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1) {
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
HAL_HSEM_Take(8,8);
HAL_Delay(1000);
HAL_HSEM_Release(8, 8);
HAL_Delay(1000);
}I've just picked a random semaphore, so number 8, out of 31.
From the comments in hal_hsem.c this is what I could gather about the usage. I've implemented the handler at the bottom of the same file:
void HAL_HSEM_FreeCallback(uint32_t SemMask){
HAL_GPIO_TogglePin(GPIOI, GPIO_PIN_14);
}My problem is the callback is never called, implying the interrupt is not firing.
2019-12-20 9:25 AM
Hello @savvn001 ,
It is preferable to keep your initial post and add a reply where you provide your finding.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.