cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G071RB INIT bit in ICSR RTC reg

wuio
Associate II

hello, after configuring the rtc in the cube the clock does not start. The initialization procedure calls the error handler. I checked that the RTC_EnterInitMode function is a problem. The INIT bit in the ICSR register is not set. Rule SET_BIT (hrtc-> Instance-> ICSR, RTC_ICSR_INIT); did not work. What could be the reason?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User

PWR_CR1.DBP not being set?

JW

wuio
Associate II

I checked this bit and it is set before the initialization. Do you have maybe STM32G071 and could you check if you are running RTC?

waclawek.jan
Super User

Indeed, the G0 has a RCC_APBENR1.RTCAPBEN bit, this is not present in any other family AFAIK.

[EDIT]

The older 'F74x does not have it, but the 'F767 does. Similarly, in the 'L4xx subfamily, the oldest 'L476 does not have it. It's also in the 'H7. In some models it is by default set, in others it is not.

JW