Skip to main content
Dmitrij Rajkov
Associate II
April 23, 2017
Question

STM32CubeMX: what kind of discovery board is meant?

  • April 23, 2017
  • 2 replies
  • 1056 views
Posted on April 23, 2017 at 21:13

I wanted to create a project for STM32F407G-DISC1 board (STM32F4DISCOVERY?) but saw two identical lines in the selection dialog (see attach).

What kind of discovery board is meant? Or is t

his mistake?

STM32CubeMX 4.20.1.

#stm32f4discovery #stm32cubemx #discovery
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
April 23, 2017
Posted on April 24, 2017 at 01:04

These are equivalent

STM32F407G-DISCO

STM32F407G-DISC1

STM32F4DISCOVERY

The DISC1 has the larger STM32F103 for the ST-LINK, supporting the mbed firmware

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Max
ST Employee
April 24, 2017
Posted on April 24, 2017 at 05:03

They are the same except for the embedded STLink version (V2: debug only or V2-1: debug, virtual COM port, mass storage).

You can see that by clicking the 0690X00000603VdQAI.jpgbutton.

BR

Max