Skip to main content
Semer CHERNI
ST Employee
November 27, 2024
Question

STM32CubeMX 6.13.0 released

We are pleased to announce to you that the release 6.13.0 of STM32CubeMX is available.

What is new in 6.13.0:

  • Added support for the following series, microcontrollers and microprocessors: STM32N6, STM32U3, STM32WL3x, STM32G411xx and STM32C0
  • Added the support for the following Nucleo boards: NUCLEO-N657X0-Q, NUCLEO-C051C8, NUCLEO-C092RC, NUCLEO-U385RG-Q, NUCLEO-WL33CC1 and NUCLEO-WL33CC2
  • Added the support for a new Discovery kits and a new expansion boards: STM32N6570-DK and B-WBA5M-WPAN
  • Extended the implementation of the CMake and Makefile build generators taking into account the memory management tool (MMT) features:
    • Single-core microcontrollers without Arm® TrustZone®(a), excluding STM32H7Rx/7Sx, or with disabled TrustZone®
    • Dual-core microcontrollers without TrustZone® (such as in the STM32H7 series)
  • Add the support of the memory management tool on STM32H7 dual-core and STM32WBA5Mxx microcontrollers
  • Added the compare projects feature to make user able to differentiate between two STM32CubeMX project files across different microcontrollers and microprocessors.
  • Implemented the loading of the firmware or applications code from the external memory (EXTMEMLOADER) using the OpenBootloader interface for STM32H7Rx/7Sx.

Main fixed issues in 6.13.0:

Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/Category:STM32CubeMX_errata

Known problems and limitations:

Refer to the STM32 microcontroller wiki at:

https://wiki.st.com/stm32mcu/wiki/STM32CubeMX_errata_6.13.x

How to get STM32CubeMX 6.13.0:

  • Under this link
  • Or update your current installation of STM32CubeMX using: Help > Check for updates
This topic has been closed for replies.

5 replies

Andrew Neil
Super User
November 27, 2024

@Semer CHERNI wrote:

Main fixed issues in 6.13.0:

Refer to the STM32 microcontroller wiki at:
https://wiki.st.com/stm32mcu/wiki/Category:STM32CubeMX_errata


There is no Errata for v6.13.0:

AndrewNeil_0-1732699860263.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TLI.11
ST Employee
December 3, 2024
MQi.1
Senior II
December 9, 2024

When downloaded the latest version here - https://www.st.com/en/development-tools/stm32cubemx.html, ant unzip it on Ubuntu, got these:

 

 

unzip en.*.zip
Archive: en.stm32cubemx-lin-v6-12-0.zip
 End-of-central-directory signature not found. Either this file is not
 a zipfile, or it constitutes one disk of a multi-part archive. In the
 latter case the central directory and zipfile comment will be found on
 the last disk(s) of this archive.
unzip: cannot find zipfile directory in one of en.stm32cubemx-lin-v6-12-0.zip or
 en.stm32cubemx-lin-v6-12-0.zip.zip, and cannot find en.stm32cubemx-lin-v6-12-0.zip.ZIP, period.

 

 

how to fix it?

Associate
December 30, 2024

Hello Semer Cherni,

STM32CubeMX 6.13.0 "Known problems and limitations" fails to point out that dual-core mcus are still not fully supported (development and debugging)

Please see: https://community.st.com/t5/stm32cubemx-mcus/stm32h7-dual-core-support/td-p/215764

Not having all the boot modes defeats the purpose of having CubeMX because the changes have to be manually remade in the IDE everytime a small change is made in CubeMX.

 

 

MKanc.1
Associate III
January 27, 2025

NUCLEO-U385RG-Q ??