Question
SAI Interface configuration small lack
Hi all,
I have noted a lack in CubeMX SAI configuration. When the interface is configured as a Master, it is only possible to set frame length to a power of two from the drop-down list. Despite when I configure it manually to 20 (I need this to implement XY100 interface, and it is one of the standard frame lengths for SAI also), it works perfectly.
In Slave mode, frame length is freely configurable.
Regards,
Dmitry