Skip to main content
JAzri.1
Visitor II
May 8, 2020
Solved

NRST stuck in reset_state

  • May 8, 2020
  • 1 reply
  • 1400 views

Hello,

I am assigning pins on a STM32F446 micro in cubemx.

I would like to give a pin name to NRST, but it is stuck in a reset_state, and won't let me change it. It is colored differently than other pins.

0693W000000X8fSQAS.png

Is it possible to change NRST, or does it stuck like that to signify that it is the reset pin? Still going to use it as the reset pin, but not sure if that has to be specified somehow.

I have the same exact issue with the BOOT0 pin. Is it possible to change the BOOT0 pin?

This topic has been closed for replies.
Best answer by Tesla DeLorean

Perhaps look at a data sheet.

The NRST and BOOT0 pins are not assignable.

NRST will be stuck low if you failed to connect VDDA​

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 8, 2020

Perhaps look at a data sheet.

The NRST and BOOT0 pins are not assignable.

NRST will be stuck low if you failed to connect VDDA​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..