My ADC reading problem with DMA
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-10-02 3:00 AM
Hello, I am working with the STM32F429-DISC1 development board. I am trying to read two adc from one channel. I can't read the code that I could read in the past. The code that worked in the morning is not working now. I may have changed a little. Please help me. My code is at below:
#include "main.h"
#include "cmsis_os.h"
#include "usb_host.h"
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
CRC_HandleTypeDef hcrc;
DMA2D_HandleTypeDef hdma2d;
I2C_HandleTypeDef hi2c3;
LTDC_HandleTypeDef hltdc;
SPI_HandleTypeDef hspi5;
TIM_HandleTypeDef htim1;
UART_HandleTypeDef huart1;
SDRAM_HandleTypeDef hsdram1;
osThreadId defaultTaskHandle;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_CRC_Init(void);
static void MX_DMA2D_Init(void);
static void MX_FMC_Init(void);
static void MX_I2C3_Init(void);
static void MX_LTDC_Init(void);
static void MX_SPI5_Init(void);
static void MX_TIM1_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_ADC1_Init(void);
void StartDefaultTask(void const * argument);
#define BufferSize 2
uint32_t adcBuff[BufferSize] = {0};
uint32_t adcData[BufferSize] = {0};
uint16_t convEnd = 0;
uint32_t voltage;
uint32_t current;
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
if(hadc == &hadc1)
{
for(int i = 0; i < BufferSize ; i++)
{
adcData[i] = adcBuff[i];
}
convEnd=1;
}
}
void ADC_Read()
{
if(convEnd==1)
{
voltage = adcBuff[0];
current = adcBuff[1];
}
convEnd=0;
HAL_Delay(5);
}
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DMA_Init();
MX_CRC_Init();
MX_DMA2D_Init();
MX_FMC_Init();
MX_I2C3_Init();
MX_LTDC_Init();
MX_SPI5_Init();
MX_TIM1_Init();
MX_USART1_UART_Init();
MX_ADC1_Init();
osThreadDef(defaultTask, StartDefaultTask, osPriorityNormal, 0, 4096);
defaultTaskHandle = osThreadCreate(osThread(defaultTask), NULL);
osKernelStart();
HAL_ADC_Start_DMA(&hadc1,(uint32_t *)adcBuff,BufferSize);
while (1)
{
ADC_Read();
}
}
- Labels:
-
ADC
-
DMA
-
STM32CubeMX
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-10-02 5:14 AM
Please help me
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-10-02 7:31 AM
The buffer is being read when the ADC completes conversion of the first channel.
Read when when the DMA count goes to zero.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-10-02 8:11 AM
Can you please explain more detailed?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-10-02 1:43 PM
Differences I have seen with the F429DISC1 HAL Library ADC DMA example:
Scan Conversion Mode is Disabled
End of Conversion Selection is Disabled.
Did you modify one or both of those?
Insert a breakpoint in the void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
function to see if this gets executed. If it doesn't, an ADC1_DMA_IRQHandler interrupt handler may be missing.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-10-05 2:51 PM
I was reading adc values with same setting, ı dont know why this is happening.