I have trouble getting ADC DMA working in cubeIDE 1.9. It was working in version 1.7
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-21 4:45 AM
There are many guides available online that explain how to set up DMA with ADC. I followed such a guide in version 1.7 and it worked out of the box. Now I'm trying the same thing in version 1.9 and it won't work.
The first thing I noticed that the ADC Clock Prescaler setting seems to be no longer a thing.The last time I set it up, I just chose continuous conversion with a prescaler and everything worked. Even without an timer. These were my settings back then:
Note here that it is the same MCU on the same board in the same project. I only updated the cubeIDE.
I now tried it with a timer (which is preferred anyway) but this still doesn't work. The timer works as can be seen on the oscilloscope here:
The yellow line is the timer, the blue line should have a peak triggered in the convCplt interrupt. DMA is set up with a circular buffer.
Here is the setup:
- https://github.com/TimGoll/masterthesis-lcr_driver/blob/main/Core/Code/Threads/AnalogIn.c#L10-L15
- https://github.com/TimGoll/masterthesis-lcr_driver/blob/main/Core/Code/Logic/AnaRP.c#L3-L8
- https://github.com/TimGoll/masterthesis-lcr_driver/blob/main/Core/Src/main.c#L101
I'd really appreciate any input on this because at this point I'm not sure if I'm doing something wrong, or if there is a bug in the cubeIDE.
MCU: STM32H743ZI on a nucleo board.
Solved! Go to Solution.
- Labels:
-
ADC
-
DMA
-
STM32CubeMX
-
STM32H7 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-21 6:03 AM
Sounds like this CubeMX code generation bug again:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-21 6:03 AM
Sounds like this CubeMX code generation bug again:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-21 7:11 AM
Thanks a lot, this means it's not me. But since this is known since a month with no announced update so far I have to wonder what the next step would be. Downgrade the IDE version? This could cause problems with ST-Link. But waiting a few weeks is no option either.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-21 7:16 AM
It’s likely to be longer than a few weeks.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-04-21 7:50 AM
For anyone else reading this: I downgraded to version 1.7.0 again. Since my ioc file was updated to 1.9.0 it was no longer readable. I therefore had to change the version flags in it and everything seems to be fixed:
Thank you again TDK. I'm a bit confused why I didn't find the open issue by myself because I did nothing but trying to solve this issue for the last two days. I honestly can't understand how a company like ST won't fix such an breaking issue within days. Or even hours. Seems highly unprofessional.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2022-06-13 2:49 PM
The GUI just does not allow me to enable Continuous DMA mode for G031 too. This problem also happens in MX. I have to downgrade to 1.8 and change ioc version too.
This bug is not small and ST may be too big that they can't handle it.