2020-12-07 2:27 AM - last edited on 2025-12-03 6:45 AM by Andrew Neil
I generated SPI1 on CubeMX. Does CubeMX SPI configuration include GPIO functionalities for the SPI pins, or do we need to programme GPIO manually?
I enabled SPI1 on CubeMX using STM32L433 on pins 11(SPI-CLK), 16(MISO), 17(MOSI). I am interfacing it to a Kionix MEMS sensor on SPI. I detect no signals on the pins. Do I need to separately write configuration for GPIO for the SPI pins?
I could not find any code generated by MX which allocates GPIO functions, incl AF to these pins.
I am wondering if it so, why is it not a part of MX code generated?
2020-12-07 2:32 AM
Dear @NAnand1 ,
Could you please share your .ioc file ?
Thank you,
Houssem
2020-12-07 2:51 AM
2020-12-07 5:29 AM
Dear @NAnand1 ,
Thank you for your file.
The code generated by STM32CubeMX is fine because STM32CubeMX is only for configuration and you can find that SPI1 is configured in the main.c.
Otherwise in order to read/write data from/to your sensor you need to use the functions found in stm32l4xx_hal_spi.c file.
Kind regards,
Houssem
2020-12-07 6:15 AM
> I could not find any code generated by MX which allocates GPIO functions, incl AF to these pins.
It's going to be in stm32f4xx_hal_msp.c in the HAL_SPI_MspInit function. Probably not looking in the right spot.
2020-12-07 9:34 PM
Dear Houssem,
I understand your response. My question was if I need to specifically configure GPIO pins 11(SPI-CLK), 16(MISO), 17(MOSI) IN ADDTION TO code generated by CubeMX to see the clock activity on the SPI_CLK pin?
I did use the functions in the relevant HAL file. However, I do not see any activity with the scope on the CLK pin, which led me to this question.
Unfortunately there is no file stm32f4xx_hal_msp.c found anywhere in the project.
2020-12-08 12:18 AM
Dear @NAnand1 ,
Every pin support some functionality and doesn't support others.
So you can't configure a pin that doesn't support to be SPI-CLK / MOSI / MISO to do SPI functions with STM32CubeMX.
In your case you have 3 SPI so you can choose between them or you can develop it manually to create an other SPI configuration and it's called bit bang.
Here is a document describe Virtually increasing the number of serial communication peripherals in STM32 applications .
Hope that this help you.
Kind regards,
Houssem
2020-12-08 1:44 AM
Dear Houssem.
I am not able to communicate my issue properly to you. Let me try to explain again.
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_ENABLE;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}
ENABLE_KX;
KX_SendBuffer[0]= 0x00;
HAL_SPI_Transmit(&hspi1, KX_SendBuffer, 1,10);
HAL_SPI_Receive(&hspi1, (uint8_t *) &KX_receiveBuffer,4,10);
DISABLE_KX;
However, I do not see any activity on any pin like SPI_CLK, MOSI or MISO at all. (The processor is working well otherwise).. Which is why I asked if I am missing something and do I need to configure ports in addition to the code provided by MX
I hope this is clear.
PS:
My doubts came from reading an instructional lesson on the web which says clearly: (reproducing relevant part here only:) The SPI has been configured and intialized already like in my program..
"
If we begin using the SPI peripheral right after calling HAL_SPI_Init(), the peripheral will appear working from the program’s point of view, but the SPI signals will not be actually be visible on the chip pins. To fix this, we need to explicitly switch pins PA5-PA7 to the SPI mode. We will leave the PA4 pin to be a generic GPIO pin to demonstrate how to control the NSS signal manually:
14
__GPIOA_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Pin = GPIO_PIN_5 | GPIO_PIN_6 | GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_4;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);