Skip to main content
Associate
Jun 14, 2025 2:57 AM UTC
Question

How to integrate CMSIS-DSP libraries on a CMake STM32 project

Hello all

I am trying to integrate CMSIS-DSP in my CMake project. From CubeMX, I have the following options:

sanmveg_0-1749869209863.png

and I see the following folder struct:

sanmveg_1-1749869245284.png

and to include DSP folder in my project, I have done the following changes in my top level CMakeLists.txt

.... some code 

# Enable CMake support for ASM and C languages
enable_language(C ASM)

# Create an executable object type
add_executable(${CMAKE_PROJECT_NAME})

# Add STM32CubeMX generated sources
add_subdirectory(cmake/stm32cubemx)
add_subdirectory(Drivers/CMSIS/DSP/Source)

# Link directories setup
target_link_directories(${CMAKE_PROJECT_NAME} PRIVATE
 # Add user defined library search paths
)

# Add sources to executable
target_sources(${CMAKE_PROJECT_NAME} PRIVATE
 # Add user sources here
 ${CMAKE_SOURCE_DIR}/Core/Src/tm1638.c
)

# Add include paths
target_include_directories(${CMAKE_PROJECT_NAME} PRIVATE
 # Add user defined include paths
 # Include CMSIS core headers
 ${CMAKE_SOURCE_DIR}/Drivers/CMSIS/Include
 ${CMAKE_SOURCE_DIR}/Drivers/CMSIS/DSP/Source
)

# Add project symbols (macros)
target_compile_definitions(${CMAKE_PROJECT_NAME} PRIVATE
 # Add user defined symbols
)

# Add linked libraries
target_link_libraries(${CMAKE_PROJECT_NAME}
 stm32cubemx
 
 # Add user defined libraries
 CMSISDSP
)

..... more code

 

However, while performing add_directory for DSP, I get the following error

[cmake] Build type: Debug
[cmake] CMake Error at Drivers/CMSIS/DSP/Source/CMakeLists.txt:12 (include):
[cmake] include could not find requested file:
[cmake] 
[cmake] configLib
[cmake] 
[cmake] 
[cmake] CMake Error at Drivers/CMSIS/DSP/Source/BasicMathFunctions/CMakeLists.txt:5 (include):
[cmake] include could not find requested file:
[cmake] 
[cmake] configLib
[cmake] 
[cmake] 
[cmake] CMake Error at Drivers/CMSIS/DSP/Source/BasicMathFunctions/CMakeLists.txt:6 (include):
[cmake] include could not find requested file:
[cmake] 
[cmake] configDsp
[cmake] 
[cmake] 
[cmake] CMake Error at Drivers/CMSIS/DSP/Source/BasicMathFunctions/CMakeLists.txt:34 (configLib):
[cmake] Unknown CMake command "configLib".
[cmake] 
[cmake] 
[cmake] -- Configuring incomplete, errors occurred!
[proc] The command: "C:\Program Files\CMake\bin\cmake.EXE" -DCMAKE_BUILD_TYPE=Debug 

Question is, am I configuring anything wrong in CubeMX? From where should I bring configDSP and configLib?

4 replies

BMcDo.3
Associate III
Jun 25, 2025 10:28 PM UTC

I'm working on this now, too (except using VSCode w/ extensions instead of STM32CubeIDE).

 


@sanmveg wrote:

Question is, am I configuring anything wrong in CubeMX?

Maybe not.

 

@sanmveg wrote:

From where should I bring configDSP and configLib?


I suspect STM32CubeMX is probably giving you Drivers/CMSIS/DSP/Source/configDsp.cmake, but if not, you can find that here:

STM32CubeF4/Drivers/CMSIS/DSP at v1.28.2 · STMicroelectronics/STM32CubeF4

 

Seems somethings got lost in migration. You should find the missing files here:

CMSIS_5/CMSIS/DSP at 5.9.0 · ARM-software/CMSIS_5

such as

Drivers/CMSIS/DSP/configCore.cmake
Drivers/CMSIS/DSP/configLib.cmake
Drivers/CMSIS/DSP/Toolchain/*.cmake

I believe you'll need to set() the variables that they and the CMakeLists.txt files need (e.g. in your CMakeLists.txt), something like

 

set(PROJECTNAME CMSISDSP)
set(ROOT "${CMAKE_CURRENT_LIST_DIR}/Drivers")
set(ARM_CPU cortex-m4)

# set only ONE of these, according to your compiler
set(GCC 1)
set(ARMAC5 1)
set(ARMAC6 1)
set(ICCARM 1)

before you

add_subdirectory(Drivers/CMSIS/DSP/Source)

 

See Drivers/CMSIS/DSP/Source/CMakeLists.txt and the *.cmake files for the variables they consume/expect.

BMcDo.3
Associate III
Jun 25, 2025 10:46 PM UTC
BMcDo.3
Associate III
Jun 25, 2025 11:46 PM UTC

I edited to add a line

set(ARM_CPU cortex-m4)

in my post above.

whitehorsesoft
Associate III
Dec 23, 2025 5:17 AM UTC

Another approach I've had luck with is to add the CMSIS-DSP packs as software packs (CMSIS-Pack) in STM32CubeMX. Here are the directions:

  1. Get both the CMSIS Core and the CMSIS-DSP packs.
    1. I'd recommend downloading the Core pack from https://www.keil.arm.com/packs/cmsis-arm/overview/ and the DSP pack from https://www.keil.arm.com/packs/cmsis-dsp-arm/versions/.
  2. Add the packs as per UM1718 § 3.4.5.
    1. If downloaded as recommended in step 1.a., install "From local".
  3. Select and enable the new software component as per UM1718 § 10.
  4. Generate code as normal
    1. Well, almost "as normal." For me this does not work with "Copy only the necessary library files" in the code generator section - instead I choose "copy all files" or "copy references" instead (ref UM1718 § 4.11.2), which seems to work fine.
  5. Open and make generated CMake project as normal - the CMakeLists.txt works fine as generated.
  6. Edit code and build.
    1. For example, I'm able to add and use arm_cos_f32 just fine.
    2. Various SIMD instructions are also available, ref https://arm-software.github.io/CMSIS-DSP/latest/group__groupExamples.html.

I'm using the CMake toolchain IDE instead of STM32CubeIDE because of its excellent integration with JetBrains CLion.

Tested with CubeMX v 6.16.0.