Skip to main content
Andrew Neil
Super User
January 14, 2025
Solved

How to have CubeMX configure a peripheral but NOT enable it?

  • January 14, 2025
  • 3 replies
  • 1236 views

I think it's a common scenario to have (at least some) peripherals which are not enabled until needed?

Or, perhaps, just configured at start-up, but not enabled until actually needed.

eg, an RTC alarm.

But CubeMX doesn't seem to support this:

  • If you don't enable the peripheral/feature, it won't let you configure it;
  • If you do enable it, it will be enabled at startup - no option to leave it til "later"

Or have I missed something/?


(none of the available tags seems appropriate, so 'Bug Report' chosen as least inappropriate. I'm using F0, but this seems to be general Cube MX behaviour - not specific to any series)

This topic has been closed for replies.
Best answer by KnarfB

STM2CubeMX Project Manager Advanced Settings has "Do not generate function call" options for the various _Init functions. 

hth

KnarfB

 

3 replies

ST Technical Moderator
January 14, 2025

Hello @Andrew Neil ,

Thank you for rising this up.

I escalated your request internally to take a closer look at the problem (via Internal ticket number: 200359).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
KnarfB
KnarfBBest answer
Super User
January 14, 2025

STM2CubeMX Project Manager Advanced Settings has "Do not generate function call" options for the various _Init functions. 

hth

KnarfB

 

Andrew Neil
Super User
January 14, 2025

Ah yes - that's it!

 

AndrewNeil_1-1743521006179.png

 

Although, in the specific case of the RTC alarm, it still just creates one MX_RTC_Init function - whereas I'd have thought it more likely that you'd want to configure and start the RTC itself separately from setting an alarm?

But that's a different question ...

 

EDIT: New question here: https://community.st.com/t5/stm32cubemx-mcus/configure-rtc-alarm-separately-from-rtc/m-p/761701 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.