Skip to main content
TDJ
Senior III
January 3, 2025
Question

CubeMX RTC config issues

  • January 3, 2025
  • 5 replies
  • 2854 views

Trying to to set up RTC alarm for STM32U5G9 I come across this CubeMX issues:

There is no option to disable Calendar date and time setup. Needless to say, probably it does not make any sense to set up date and time on every board reset if it has (as it should) some RTC battery backup.
It is not a big deal until one configures RTC alarm, function "return" statement can be added in MX_RTC_Init() 'user code' section before date/time gets reconfigured.
However, this is not an option when RTC alarm is configured because code execution needs to reach this part resetting time and date along the way.

Another reason for that is the lack of 'user code' between date/time setup and alarm setup sections in generated code. Otherwise, label and goto statement could be used to skip date/time setup.

I find lack of an option to disable date/time config very annoying. Probably this feature was never implemented because originally CubeMX was meant only to generate "quick and dirty" demo code so it did not matter.

TDJ_1-1735906003846.png

TDJ_2-1735907337800.png

 

This topic has been closed for replies.

5 replies

ST Employee
January 6, 2025

Hello @TDJ

A solution I can think of, is to use the backup registers to store a flag indicating whether the RTC has been initialized; 

So, the code first checks if the RTC is already running by reading a specific flag from the backup register (`RTC_BKP_DR1`). If the flag is set (e.g., `0x1234`), it means the RTC has been initialized previously, and the function returns early to skip the date/time setup. If not -the RTC is not initialized- the code proceeds to initialize the RTC and set the date and time then configures the RTC alarm. 

The flag indicating that the RTC has been initialized should be in the backup domain, so it will be retained at reset. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
TDJ
TDJAuthor
Senior III
January 6, 2025

Hello @Sarra.S I tried to explain why the approach you suggested is not doable if an RTC alarm is also configured. Simply, there is no way to place code in the 'user code' section that will conditionally or unconditionally skip the date/time config and go straight to RTC alarm config. There is not 'user code' section between date/time setup and RTC alarm config where code execution could jump to in order to skip date/time setup - no matter what the logic behind is.
I can see two solutions which are not mutually exclusive:
1. Make CubeMX current date/time config optional. It is current date/time. Usually, other than for Nucleo boards without battery used for demo, there is no need to hardcode it.
2. In the generated code add another 'user code' section between date/time config and RTC alarm config code

TDJ
TDJAuthor
Senior III
January 10, 2025

@Sarra.S Maybe this picture below will better illustrate the problem.

TDJ_0-1736522574722.png

 

ST Employee
January 13, 2025

Hello @TDJ

Thank you for explaining the issue, I have submitted a ticket to address the problem (Internal ticket number: 200239). 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
January 15, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.