Skip to main content
Associate III
December 11, 2023
Solved

CubeMX generates incorrect code for the STM32U575 MDF peripheral for multiple filters using DMA

  • December 11, 2023
  • 3 replies
  • 1760 views

I am working with the MDF peripheral and find this to be a great peripheral. However the CubeMX generated code for multiple DMA based filters is not correct.


I am using two filters with DMA and CubeMX generates the following descriptors:

  1. MDF_HandleTypeDef MdfHandle0;
  2. MDF_FilterConfigTypeDef MdfFilterConfig0;
  3. MDF_HandleTypeDef MdfHandle1;
  4. MDF_FilterConfigTypeDef MdfFilterConfig1;
  5. DMA_NodeTypeDef Node_GPDMA1_Channel1;
  6. DMA_QListTypeDef List_GPDMA1_Channel1;
  7. DMA_HandleTypeDef handle_GPDMA1_Channel1;
  8. DMA_NodeTypeDef Node_GPDMA1_Channel0;
  9. DMA_QListTypeDef List_GPDMA1_Channel0;
  10. DMA_HandleTypeDef handle_GPDMA1_Channel0;

 

When starting the application I found that both MdfHandle0 and MdfHandle1 refer the same DMA handle,  handle_GPDMA1_Channel1. Likewise both handle_GPDMA1_Channel0.Parent and handle_GPDMA1_Channel1.Parent refer the same filter handle,  MdfHandle0.

This is caused by generated function HAL_MDF_MspInit which is called when starting a filter using HAL_MDF_AcqStart_DMA. This generated function is executed twice since I use two filters but inside this function the exact same code is executed and no distinction is made whether it is called for filter 0 (MdfHandle0) or filter 1 (MdfHandle1).

In other generated ....MspInit functions a distinction is made based on the peripheral instance the function is called for. For instance for UART's in my code, HAL_UART_MspInit looks like:

...

if(huart->Instance==LPUART1)
{

...;

}

else if(huart->Instance==USART1)

{

...;

}

In order to differentiate between the different UART instances.

 

This however is not done in HAL_MDF_MspInit. Instead of the above use is made of:

if(IS_MDF_INSTANCE(hmdf->Instance)) which is typically used inside the HAL but not in the generated code and using this no different code is generated for the different filter instances.

The same issue applies to HAL_MDF_MspDeInit.

 

I have set the wrong descriptors correct manually after the CubeMX initialization code and everything works as expected.

I am using version 6.10.0 of CubeMX and version 1.4.0 of the STM32U5xx HAL library.

 

Best answer by Souhaib MAZHOUD

Hello all,

Issue is fixed in the latest STM32CubeMX release 6.17.0 available here.

KR, Souhaib

3 replies

ST Technical Moderator
December 13, 2023

Hello @LVan .31 

Thank you for bringing this issue to our attention, I will check it internally and get back to you as soon as possible.

Thx

Souhaib

 

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
LVan .31Author
Associate III
July 4, 2024

I really love the software ST provides nowadays. I remember the time (not that long ago) that chip manufacturers did offer very limited software support. Their business was selling chips and the programming was left to the customer. Most manufacturers have come a long way since then......... but.........

When customers report bugs in the software and since the time of reporting two new versions of the software (CubeMX in this case) have emerged I think it is quite annoying that the issues are not solved. The issue reported in the original post still exists and I have not heard or seen any reaction since the end of 2023 when this issue was reported.

The issue is a serious bug in the CubeMX generated code for the MDF peripheral. I use two filters each having its own DMA channel. Not only is the complete initialization code for the MDF filters executed twice in this case (or even more often when using more filters) but, and this is the bug, all filters are set to the same DMA channel leading to an error when running the code since the same channel is started more than once. My workaround is that in the user code at the end of the generated function I have added:

 

 

 

/* USER CODE BEGIN MDF1_MspInit 1 */
if (hmdf->Instance == MDF1_Filter0)
{
 __HAL_LINKDMA(hmdf, hdma, handle_GPDMA1_Channel0);
}
else
{
 __HAL_LINKDMA(hmdf, hdma, handle_GPDMA1_Channel1);
}

/* USER CODE END MDF1_MspInit 1 */

 

 

to set the desired DMA channel to the correct filter but for sure this is not what you want. The call to __HAL_LINKDMA is already present in the generated code and my workaround just overwrites this.

 

Please ST, is it possible to be more responsive...............

 

 

Associate
August 21, 2025

I am working on a new project where an important role is for the STM32U575 MDF filter using multiple channels.

The issue reported above still exists in the most current version of the Cube generated code. This is really annoying.

void HAL_MDF_MspInit(MDF_HandleTypeDef* hmdf)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 DMA_NodeConfTypeDef NodeConfig;
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 if(IS_MDF_INSTANCE(hmdf->Instance))
 {

In the code generated in the above code snippet line 6 tests if this function is called for one of the filters in the MDF but next the code following is not specific for each of the MDF filters but the same, regardless which filter this function is called for.  So for every filter the GPIO's are initialized, the MDF clock is activated and so on. This is just redundancy. But what is worse is that the filter specific DMA settings  overwrite each other and the last call wins. So when using multiple filters, each with its own DMA channel, the last DMA wins and is used for all filter that are already initialized.

 

This code is just wrong, the error is reported something like 2 years ago and still nothing happens.

When will this issue be fixed, MDF is a great peripheral but the generated code is not!!!!! 

stst9180
Associate III
November 19, 2025

Same here. This is annoying. Please fix this issue. 
We currently use CubeMX for generating code that is "not touched at all" and on every build process code is regenerated. This bug needs manual patching currently which is always a mess.

 

Regards Pascal

Associate
November 19, 2025

I fixed the issue temporary by adding user code for my specific situation. This user code just sets the desired DMA channels on every call to HAL_MDF_MspInit so I don't have to change the code on every regenerate.

 /* USER CODE BEGIN MDF1_MspInit 1 */

 extern MDF_HandleTypeDef MdfHandle0;
 extern MDF_HandleTypeDef MdfHandle3;


 __HAL_LINKDMA(&MdfHandle0, hdma, handle_GPDMA1_Channel4);
 __HAL_LINKDMA(&MdfHandle3, hdma, handle_GPDMA1_Channel5);

 /* USER CODE END MDF1_MspInit 1 */

 

ST Technical Moderator
November 19, 2025

Hello @Leon3 

Thank you for posting the workaround,
In fact, this issue has been discussed internally, and the fix is currently under review. (Ticket 222109 This is an internal tracking number and is not accessible or usable by customers).)
I appreciate your understanding and I will keep you updated on any progress.

BR, Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.