Skip to main content
Max Rest
Associate II
March 11, 2019
Question

CubeMX 5.1 - CMSIS DSP library missing for Toolchain SW4STM32

  • March 11, 2019
  • 1 reply
  • 926 views

Hello STM,

when I generate a project for STM32H750 with CubeMX 5.1 with Toolchain SW4STM32 selected, CMSIS DSP library is missing from the project and it does not compile.

Also, a preprocessor define of

__ARM_ARCH_7EM__=1

is missing to specify the ARM Architecture, which leads to missing gcc intrinsics in cmsis_gcc like __SSAT and the likes.

This topic has been closed for replies.

1 reply

Ala Eddine Bakkay (Intern at A
Visitor II
March 15, 2019

Use Keil uVision is better for STM32 programming