Configuring STM32F401 USART6 for 115200 baud results in 38400 baud
- September 17, 2025
- 6 replies
- 497 views
I used STM32CubeMX to configure an STM32F401RETx USART6 for 115200 baud. I searched but could not find an example to start from. I enabled USART to register USART callbacks using the STM32MXCube Project Manager Advanced Settings. My project utilizes FreeRTOS, so I added that and created a simple default task to receive a character and output a message each time a character is received.
I used an FTDI TTL-232-RG-VIP-WE cable connected to GND, 3V3, PC6, and PC7, and to a Windows PC set for 115200/8/N/1.
At run time, I set a breakpoint where the character should appear in my receive buffer, and observed that I was getting garbage in. Also, I saw I was getting garbage out. I stepped the initialization, configuration, interrupts, and callbacks — all appeared to be working correctly.
In desperation, I experimented with the baud rate and found that I could send and receive good characters with the PC set to 38400 baud while the STM32F401 remained configured for 115200.
What is going on here? The project is attached.