Skip to main content
Marco.D
Associate II
March 4, 2021
Solved

[Bug for MPU LL code generation for H755]

  • March 4, 2021
  • 3 replies
  • 2514 views

I am using CubeIDE Version: 1.6.0 Build: 9614_20210223_1703 (UTC) to initialise the MPU as it is done for the TCP_Echoserver, however the LL resulting code does not set the LL_MPU_TEX_LEVEL1 bit for the second region

0693W000008w0bjQAA.pngGenerated code:

/* MPU Configuration */
 
void MPU_Config(void)
{
 
 /* Disables the MPU */
 LL_MPU_Disable();
 /** Initializes and configures the Region and the memory to be protected
 */
 LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER0, 0x0, 0x30000000, LL_MPU_REGION_SIZE_256B|LL_MPU_REGION_FULL_ACCESS|LL_MPU_INSTRUCTION_ACCESS_ENABLE|LL_MPU_ACCESS_NOT_SHAREABLE|LL_MPU_ACCESS_NOT_CACHEABLE|LL_MPU_ACCESS_BUFFERABLE);
 LL_MPU_EnableRegion(LL_MPU_REGION_NUMBER0);
 /** Initializes and configures the Region and the memory to be protected
 */
 LL_MPU_ConfigRegion(LL_MPU_REGION_NUMBER1, 0x0, 0x30004000, LL_MPU_REGION_SIZE_16KB|LL_MPU_REGION_FULL_ACCESS|LL_MPU_INSTRUCTION_ACCESS_ENABLE|LL_MPU_ACCESS_SHAREABLE|LL_MPU_ACCESS_NOT_CACHEABLE|LL_MPU_ACCESS_NOT_BUFFERABLE);
 LL_MPU_EnableRegion(LL_MPU_REGION_NUMBER1);
 /* Enables the MPU */
 LL_MPU_Enable(LL_MPU_CTRL_PRIVILEGED_DEFAULT);
 
}

This topic has been closed for replies.
Best answer by Khouloud OTHMAN

Hi @Community member​ ,

Thanks for your feedback. I've been able to reproduce the issue from my side and I will report it internally to be reviewed by the development team.

I will keep you posted with updates.

Even though this reply doesn’t directly solve the issue, I’m marking it as Best, since it will help clarify the current situation for other customers with the same question. I will post an update here once the issue has been fixed

Thanks for your contribution.

Khouloud.

3 replies

Khouloud OTHMAN
Khouloud OTHMANBest answer
Associate
March 4, 2021

Hi @Community member​ ,

Thanks for your feedback. I've been able to reproduce the issue from my side and I will report it internally to be reviewed by the development team.

I will keep you posted with updates.

Even though this reply doesn’t directly solve the issue, I’m marking it as Best, since it will help clarify the current situation for other customers with the same question. I will post an update here once the issue has been fixed

Thanks for your contribution.

Khouloud.

MDega.1
Visitor II
March 5, 2021

Hello Khouloud,

can you also check for the STM32H735G-DK?

For this device, with the same settings, the CubeMX doesn't seem to generate any code for the MPU at all, neither in LL nor in HAL.

 

Regards,

Marco

Sorry, don't know what happened but now it works (with the same bug as above)

Sara BEN HADJ YAHYA
ST Technical Moderator
June 29, 2022

Hello,

This issue is fixed in STM32CubeMX latest release.

V6.6.0 is now available under this Link.

Thanks for your contribution.

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.