cancel
Showing results for 
Search instead for 
Did you mean: 

6.7.0. STM32H745 doesn't have "Power Regulator Voltage Scale 0" in the list

Pavel Krupets
Associate III

I selected LDO power supply

But frequency is still limited to 400MHz.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Piranha
Chief II

Set the "Product revision" to "rev.V" and read the AN5337.

View solution in original post

6 REPLIES 6
AScha.3
Super User

try just for test: use smps supply, scale 0 should be possible then.

If you feel a post has answered your question, please click "Accept as Solution".

nope, I tried different regulators but 0 is never in the list

main thing is that according to specs 480MHz available only with LDO but no matter what I do, I couldn’t set frequency to 480.

Piranha
Chief II

Set the "Product revision" to "rev.V" and read the AN5337.

REALLY APPRECIATE YOUR HELP!!!

THAT SOLVED MY ISSUE!!!

I am on NUCLEO board, playing with collecting data, lifetime is of no concern

though ST should add this to error message when I am unable to set frequency to 480 MHz

KDJEM.1
ST Employee

Hello @Pavel Krupets​,

This issue is already reported in this post.

Sorry for this inconvenience.

Internal ticket number: 140578 (This is an internal tracking number and is not accessible or usable by customers).

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

KDJEM.1
ST Employee

Hello @Pavel Krupets​,

This issue has been solved in the STM32CubeMX6.8.0.

Thank you for your contribution.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.