Skip to main content
jumman_JHINGA
Senior III
July 5, 2023
Solved

Why STM32F207 is getting stucked in Startup file, when im generating ethernet code from CubeMx 6.8.1

  • July 5, 2023
  • 9 replies
  • 5944 views

Hello guys!

Now a days im facing issue with ethernet configuration in the latest version of CubeMx 6.8.1.

When im configuring the ethernet for my F207 nucleo board in its getting stucked into startup file. and through debugging when im pressing F5 button for manay times, then its getting out from startup file and my code starts working and getting pinged from my PC.

 

But when im generating code from CubeMx 5.4.0 version for same configuration, its working fine. im not geeting any issues with this version.

has anyone resolved this issue? 

This topic has been closed for replies.
Best answer by jumman_JHINGA

IN THE MDKARM IDE:

If MCU is getting stuck after dumping the code, then you need to Change following settings in Manage Run Time environment:

mdkarm.png

 

after doing these settings presse ok and re compile the program and dump the code now Ethernet will work perfectly. 

for IAR Workbench Ide no need to change any settings it will work. for STM Cube Ethernet will not work with latest version of CubeMx.

9 replies

ST Technical Moderator
July 6, 2023

Hello @jumman_JHINGA,

Which Cube Firmware version are you using?

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
jumman_JHINGA
Senior III
July 10, 2023

for 6.8.1 firmware version is 1.9.4 and for 5.4.0 firmware version is 1.8.0

Semer CHERNI
ST Employee
July 10, 2023

Hello @jumman_JHINGA 

Could you share the ioc so I will be able to be in the same configuration as yours. 

KR,

Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
jumman_JHINGA
Senior III
July 11, 2023

hii @Semer CHERNI Plz check this ioc file.

jumman_JHINGA
Senior III
July 27, 2023

Hi @Semer CHERNI  and @Imen.D I am waiting for your replay please help me out to find solution on this.

 

Associate III
October 23, 2023

I have similar issue on STM32F746g-disco with CubeMX 6.9.2. Is there any solution for this case?

 

jumman_JHINGA
Senior III
October 25, 2023

Hii @hbZhao ...

I'll suggest you to don't configure ethernet with latest version of CubeMX. 

You should have to configure ethernet manually using HAL libraries. 

jumman_JHINGA
Senior III
November 7, 2023

After digging more into this issue, i got to know that , after configuring Ethernet and generating the code through latest version of CubeMx then controller is not able to jump to main function.

jumman_JHINGA
jumman_JHINGAAuthorBest answer
Senior III
March 2, 2024

IN THE MDKARM IDE:

If MCU is getting stuck after dumping the code, then you need to Change following settings in Manage Run Time environment:

mdkarm.png

 

after doing these settings presse ok and re compile the program and dump the code now Ethernet will work perfectly. 

for IAR Workbench Ide no need to change any settings it will work. for STM Cube Ethernet will not work with latest version of CubeMx.