Skip to main content
DavidAlfa
Senior II
March 26, 2021
Question

Bug? CubeMX USB OTG , SOF flag causing interrupt flood (Fixed)

It only happens when there's an active transfer.

The OTG interrupt was called every 3...6uS (300-500 Core clocks @ 96MHz).

It seemed crazy excesive to me, that can't be correct!

Just to clarify: STM32F411, internal FS controller, cubeIde initialization, host mode (OTG).

Checking what interrupt flag was causing the calls, I found the culprit to be the SOF flag.

I put a small variable there and traced using SVW: 

0693W000008y2bBQAQ.png 

I have SOF disabled in CubeMX, however the code enables it anyway:

IDE: STM32Cube IDE v1.6.0
FILE: stm32f4xx_ll_usb.c
LINE: 1355
FUNCTION: HAL_StatusTypeDef USB_HostInit(USB_OTG_GlobalTypeDef *USBx, USB_OTG_CfgTypeDef cfg)
 
 
 
 USBx->GINTMSK |= (USB_OTG_GINTMSK_PRTIM | USB_OTG_GINTMSK_HCIM | \
 USB_OTG_GINTMSK_SOFM | USB_OTG_GINTSTS_DISCINT | \
 USB_OTG_GINTMSK_PXFRM_IISOOXFRM | USB_OTG_GINTMSK_WUIM);

Removing USB_OTG_GINTMSK_SOFM from the mask fixed the problem.

I'm still having interrupts every 40uS (around 3000 cpu cycles) caused by the USB_OTG_GINTSTS_RXFLVL flag.

Edit: That's correct, due the 64-byte buffer triggering the FIFO interrupt

(64 bytes = 512 bits, at USB 12MHz clock = 42uS).

However it still has does some 3-5uS ones. Not a thousand, but maybe 10 out of 20.

Maybe the interrupt is not being fast enough ?

This is a 512-bytes read:

Cycles		Timestep(uS)
3631	
4027		4,1
4455		4,5
4922		4,9
6036		11,6
21355		159,6
89994		715,0
95273		55,0
100552		55,0
104458		40,7
108230		39,3
111117		30,1
113988		29,9
123957		103,8
124385		4,5
124899		5,4
125324		4,4
130489		53,8
130917		4,5
131431		5,4
133660		23,2
137085		35,7
140378		34,3
143691		34,5
147096		35,5
148832		18,1

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
March 26, 2021

Which STM32?

Device or host?

Okay I've guessed, host.

If you have SOF interrupt more often than once in a frame (maybe microframe in HS, I don't use HS), then it's likely you've set the frame timer (OTG_HFIR) incorrectly. Observe, how fast frame number in OTG_HFNUM increments, and observe the SOF frames on the bus.

JW

DavidAlfa
DavidAlfaAuthor
Senior II
March 27, 2021

OTG, so Host mode. Internal FS controller.

Default CubeMx configuration.

I might be a debugging issue, as it seems to happen a lot more when you halt the core, I guess the USB keeps working in the background, the interrupts pile up, and when you resume it's like a tsunami.