Skip to main content
RGari
Associate II
August 10, 2019
Solved

Support for STM32H757

  • August 10, 2019
  • 1 reply
  • 884 views

When trying to generate code using STMCubeMX, both TrueStudio (understandable) and STM32CubeMXIde are greyed out. I have the newest version of CubeMX, CubeMXIde, and TrueStudio installed.

When will the 757 be supported? We are in a rush in developing a major prototype project (we have been waiting for DSI support forever on the H7 line) and now that it's available, support for it is far from complete. There seems to be no mention of it being supported or not anywhere.

Thoughts? The 753 is supported, so why not the 757? There aren't very many differences between the two parts (except for DSI and the power supply).

This topic has been closed for replies.
Best answer by mƎALLEm

Hello,

This an old thread but, STM32CubeMx, STM32CubeIDE (deprecated TrueStudio) and STM32CubeProgrammer support STM32H7 dual core years ago including  STM32H757 devices.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
September 2, 2024

Hello,

This an old thread but, STM32CubeMx, STM32CubeIDE (deprecated TrueStudio) and STM32CubeProgrammer support STM32H7 dual core years ago including  STM32H757 devices.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.