STM32U575 + FreeRTOS - waking up from Stop Mode
Using an STM32U575 on our own design. Aim is to put it into Stop2 Mode and wake up from three sources:
a) GPIO pin
b) Wake up timer (RTC)
c) AlarmA (RTC)
I have these three sources setup as interrupts and when the CPU is running (i.e. not stopped) these interrupts fire and are handled correctly. However, when entering stop mode, the device cannot be woken when any of these 'interrupts' occur - those of you familiar with this will recognise that while the interrupts don't wake up the CPU, these interrupt sources are used to wakeup the CPU when they occur after which the interrupt will be serviced.
Debugging in low power mode is troublesome, so my best insight comes from using the STM32Cube Programmer, attaching in 'hot' mode and examining the SFRs. Here I can see the WUTF and ALRMAF are set, but still no wake-up.
Frustratingly, I have used the examples referred to in this rather good tutorial and based on this I can (using a Nucleo board) enter Stop2Mode and exit is successfully using the RTC wakeup timer. I am unable to replicate this with our own hardware and project code.
So what are the differences? well, the Nucleo example is frustratingly simple:
/* Enable ultra low power mode */
HAL_PWREx_EnableUltraLowPowerMode();
/* Enable the Autonomous Mode for the RTC Stop0/1/2 */
__HAL_RCC_RTCAPB_CLKAM_ENABLE();
/* Set RTC wakeup timer for 2s */
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 2, RTC_WAKEUPCLOCK_CK_SPRE_16BITS, 0);
/* 4 - Measure consumption in Stop 2 mode Full SRAM retention */
/* Enter in Stop 2 mode */
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);
but in our code, I am using FreeRTOS which adds a further complication, but on the face of it, it should be as straightforward as with the HAL-only based example. It appears that something somewhere isn't being enabled or setup correctly. I was hoping that someone might have some insight or been where I am at the moment and escaped!
My PreSleepProcessing is getting more and more complex each day!
void PreSleepProcessing(uint32_t ulExpectedIdleTime)
{
/* Called by the kernel before it places the MCU into a sleep mode because
configPRE_SLEEP_PROCESSING() is #defined to PreSleepProcessing().
NOTE: Additional actions can be taken here to get the power consumption
even lower. For example, peripherals can be turned off here, and then back
on again in the post sleep processing function. For maximum power saving
ensure all unused pins are in their lowest power state. */
if (allow_deep_sleep == true)
{
//HAL_TIM_Base_DeInit(&htim3)
//TIM3->CCR1 &= ~0x01;
HAL_SuspendTick();
/*
(*ulExpectedIdleTime) is set to 0 to indicate that PreSleepProcessing contains
its own wait for interrupt or wait for event instruction and so the kernel vPortSuppressTicksAndSleep
function does not need to execute the wfi instruction
*/
ulExpectedIdleTime = 0;
// GPIOB->ODR |= OPTICAL_EN_Pin;
// GPIOB->ODR &= ~OPTICAL_EN_Pin;
// //GPIOB->ODR |= OPTICAL_EN_Pin;
// GPIOB->ODR &= ~OPTICAL_EN_Pin;
// Apparently this is helpful for ensuring that Stop mode is entered
HAL_PWREx_EnableUltraLowPowerMode();
// This ensures that the RTC is still clodked in stop mode
__HAL_RCC_RTCAPB_CLKAM_ENABLE();
// The following two wakeup pin enables set the RTC and PB7 (CLI) to wake up the CPU
// RM0456 Rev 3 Table 86
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN6_HIGH_3);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN7_HIGH_3);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN8_HIGH_3);
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN4_LOW_2);
// Now clear the relevant flags
__HAL_RTC_CLEAR_FLAG(&hrtc, RTC_CLEAR_WUTF);
//__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_ALL_FLAG);
if (__HAL_PWR_GET_FLAG(PWR_FLAG_STOPF) != RESET)
{
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_STOPF);
}
if (__HAL_PWR_GET_FLAG(PWR_WAKEUP_FLAG4) != RESET)
{
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_FLAG4);
}
if (__HAL_PWR_GET_FLAG(PWR_WAKEUP_FLAG7) != RESET)
{
__HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_FLAG7);
}
// This puts the CPU into stop mode
HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFE);
Thanks in advance!