cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeIDE randomly cant find header files after compiling fine for days. Very random

Beachmiles
Associate III

If I double click on the supposedly missing include file CubeIDE finds the file in the project path just fine...

I seem to have to recreate the project in MX / clean-re-build to get the libraries to re-figure out that they exist. Very strange.

Is there another non-buggy compiler that I should use that integrates with Cube ? Im on the Stm32L4 so I think I need to pay for the Keil IDE.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Markus GIRDLAND
ST Employee

Do you do anything in particular once the files "go missing"? Is it with a fresh launch of CubeIDE or something like that?