Skip to main content
PGump.1
Senior II
February 23, 2024
Question

STM32CubeIDE locks up on exit

Hi all,

The last two times I have exited from STM32CubeIDE it has locked up. Does anyone know how to fix this?

My system is Linux, Tumbleweed, Plasma (X11), Cube V14.0.

When I Exit, I get the Exit confirmation message box, I select Exit - then the my cpu goes into a 99.9% locked state, the cpu temperature goes way up, the fan turbos as fast as it can, the bios throttles back the clock in an attempt to stabilize the system. It doesn't resolve itself. I have to open a terminal and kill java.

I get this message from STM32CubeIDE -

JVM terminated. Exit code=143
/home/user/st/stm32cubeide_1.14.0//plugins/com.st.stm32cube.ide.jre.linux64_3.1.0.202310310920/jre/bin/java
-Dosgi.requiredJavaVersion=1.8
-Dosgi.instance.area.default=@user.home/STM32CubeIDE/workspace_1.14.0
-Declipse.buildId=Version 1.14.0
-DproductMaturityGrade=mm
-Djdk.http.auth.tunneling.disabledSchemes=
-XX:+UseG1GC
-XX:+UseStringDeduplication
-Xms256m
-Xmx1024m
-jar /home/user/st/stm32cubeide_1.14.0//plugins/org.eclipse.equinox.launcher_1.6.500.v20230717-2134.jar
-os linux
-ws gtk
-arch x86_64
-showsplash
-launcher /home/user/st/stm32cubeide_1.14.0/stm32cubeide
-name Stm32cubeide
--launcher.library /home/user/st/stm32cubeide_1.14.0//plugins/org.eclipse.equinox.launcher.gtk.linux.x86_64_1.2.700.v20221108-1024/eclipse_11801.so
-startup /home/user/st/stm32cubeide_1.14.0//plugins/org.eclipse.equinox.launcher_1.6.500.v20230717-2134.jar
--launcher.overrideVmargs
-exitdata 10010
-vm /home/user/st/stm32cubeide_1.14.0//plugins/com.st.stm32cube.ide.jre.linux64_3.1.0.202310310920/jre/bin/java
-vmargs
-Dosgi.requiredJavaVersion=1.8
-Dosgi.instance.area.default=@user.home/STM32CubeIDE/workspace_1.14.0
-Declipse.buildId=Version 1.14.0
-DproductMaturityGrade=mm
-Djdk.http.auth.tunneling.disabledSchemes=
-XX:+UseG1GC
-XX:+UseStringDeduplication
-Xms256m
-Xmx1024m
-jar /home/user/st/stm32cubeide_1.14.0//plugins/org.eclipse.equinox.launcher_1.6.500.v20230717-2134.jar

Kind regards

PG

 

This topic has been closed for replies.