Skip to main content
Leopold N.
Associate II
May 1, 2020
Question

STM32CubeIDE Disassembly Error

  • May 1, 2020
  • 0 replies
  • 991 views

Hello,

i use STM32CubeIDE to program STM32H753 and i now got this error in my disassembly (attached).

The Code Piece is attached too.

I tried a bit and have seen that the error only occurs when i add the for-loop. Without it, its all ok. When i move the for-loop out of the if-break, its ok too.

The error occurs because the debugger tries to read from address 0x00010000, which doesnt exist physically (ITCM ends at 0x0000FFFF). But i dont know, why the debugger accesses that address.

I attached the debug log too.

Anyone an idea?

Greetings

This topic has been closed for replies.