Skip to main content
Senior
February 25, 2025
Solved

St-Link is not detected MacOS 15.3.1

  • February 25, 2025
  • 6 replies
  • 3058 views

Hello,

I update my computer to MacOs 15.3.1 and I have a similar problem to when MacOs 15 arrived. The St-Link (ST-Link v3 mini) is not detected with Cube IDE (CubeIDE v. 1.17.0).
It worked fine in MacOS 15.1.1

I've tried starting the IDE as admin and adding the link's path to the path list, but it doesn't work. (https://community.st.com/t5/stm32cubeide-mcus/stlink-server-with-macos-15/td-p/705089)


On the other hand, it is well detected with STM32Programmer.

I added the IDE to the development tools in the security tab of the computer settings, just in case the problem came from the fact that apple could have changed the security rules, but that didn't solve the problem.

 

This topic has been closed for replies.
Best answer by MA4

I called Apple support and they told me there must be a problem with the Mac update and the stm32Cube IDE application. I reinitialized my computer (deleting the entire disk and reinstalling Sequoia with the recovery mode) and it's working again (with MacOS 15.3.2).
If you try to delete your disk keep a save in an external drive thanks to Time Machine just in case.

6 replies

ST Technical Moderator
February 26, 2025

Hello @MA4 


Could you please take a look at this FAQ . The workarounds could be a solution to your problem.

 

BR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
MA4Author
Senior
February 27, 2025

Hello,

Thank you for our answer.

I'm not sure if it's USB related cause it was working before I updated my OS. It also works with STM32Programmer, I only have the issue with STM32CubeIDE

MA4Author
Senior
March 11, 2025

Update my IDE to 1.18 doesn't fix. 
I think I'm gonna downgrade my OS.

Visitor II
March 23, 2025

Hi all,

 

I'm using macos 15.3 and my stm32H7S78 discovery board doesn't want to download. I think i'm running into the same problem as you guys, anybody who found a fix?

 

thx in advance.

MA4AuthorBest answer
Senior
March 26, 2025

I called Apple support and they told me there must be a problem with the Mac update and the stm32Cube IDE application. I reinitialized my computer (deleting the entire disk and reinstalling Sequoia with the recovery mode) and it's working again (with MacOS 15.3.2).
If you try to delete your disk keep a save in an external drive thanks to Time Machine just in case.

Visitor II
March 26, 2025

Yeah eventuallly i got it working yesterday, all i had to do was use an old usb splitter to force usb 2.0 and then suddenly everything in cubeprogrammer worked. 

cubeIDE still doesn't seem to work but i can life with that.

Now i just need to figure out how i can consistenly compile the boot and application files :)) my normal workflow with cmake doesn't seem to like this and cube ide works about 1/10 times.