Setup for ISPU Core workshop fails
I'm trying to do the ISPU workshop and using STM32CubeIDE fails trying to use the projects loaded from the file system. I can load the program, the program properties, build settings need to be changed and while everything looks good it won't compile due to not finding stdbool.h, math.h and stdint.h. This has got to be an easy fix, but elusive. These files are not found on the win10 machine and I'm at a loss to figure out what needs to be loaded to provide these files. The win10 CubeIDE install is fresh (done it twice) and all the requisites for the workshop are installed and apparently show up as available using the workshop validator. The kicker is that the whole installation done with Linux works perfectly and without issue but unfortunately the workshop requires Unicleo which isn't available for Linux.
Thanks,
TJM