Skip to main content
Associate
Sep 17, 2024 7:01 AM UTC
Question

Search: An internal error occurred during: "File Search Worker".

When I execute a text search in the Stm32CubeIDE Version: 1.16.0
Build: 21983_20240628_1741 (UTC) the following error appears:
 
Problems encountered during text search.
An internal error occurred during: “File Search Worker”.
'byte[] org.eclipse.core.resources.IFile.readNBytes(int)'
 
The error log then reads:
!SUBENTRY 1 org.eclipse.core.jobs 4 2 2024-09-17 08:36:23.077
!MESSAGE An internal error occurred during: “File Search Worker”.
!STACK 0
java.lang.NoSuchMethodError: 'byte[] org.eclipse.core.resources.IFile.readNBytes(int)'
at org.eclipse.search.internal.core.text.FileCharSequenceProvider.toShortString(FileCharSequenceProvider.java:495)
at org.eclipse.search.internal.core.text.FileCharSequenceProvider.newCharSequence(FileCharSequenceProvider.java:42)
at org.eclipse.search.internal.core.text.TextSearchVisitor$TextSearchJob.processFile(TextSearchVisitor.java:208)
at org.eclipse.search.internal.core.text.TextSearchVisitor$TextSearchJob.run(TextSearchVisitor.java:173)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)
 
This error occurred suddenly
 
What can do to solve this Problem ?
This topic has been closed for replies.

5 replies

Visitor II
Sep 17, 2024 7:15 PM UTC

this started happening to me after installing a Copilot plugin from Eclipse marketplace.

Uninstalling the plugin didn't help.

I reinstalled eclipse and this fixed the problem.

Associate II
Sep 18, 2024 6:11 AM UTC

hi,

 

was it this one? https://marketplace.eclipse.org/content/copilot4eclipse

i have the same problem, also installed this plugin and it happened all of a sudden. for some time it did work. i did not change anything and *poff* i got this error

i have the same error in another eclipse based IDE (where i also installed this plugin)
in the beginning it worked flawlessly 

Associate
Sep 18, 2024 6:29 AM UTC

Ok, I had also installed the Copilot plugin. At the beginning everything worked and then yesterday suddenly this error message when searching.
Now I have reinstalled the CubeIde, but still without Copilot Plugin, at the moment the search function works again.

Semer CHERNI
ST Employee
Sep 25, 2024 1:05 PM UTC

Hello

Thanks for posting :).

The copilot plugin for Eclipse is not compatible with the Eclipse CDT version on which STM32CubeIDE is based.

The investigation is ongoing internally and it should be fixed when the Eclipse version used by STM32CubeIDE is upgraded. This will be included in future releases.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Sep 25, 2024 1:08 PM UTC

hi,

there was an update from Genuitec. This posting explains the details. With this version it should be fixed

https://github.com/Genuitec/Copilot4Eclipse-community/discussions/23