cancel
Showing results for 
Search instead for 
Did you mean: 

Project dont work after migrating to STM32G4 package version 1.3.0 and CubeIDE 1.4.0

KoRba88
Associate III

Hi

My project was ok before, on 1.2.0 package version and CubeIDE 1.3.0. After migrating ADC 2,3,4,5 dont work (STM32G474QE). Im use LL and CMSIS

In my project i have ADC with DMA and triggered ADC1 &ADC5 from the same HR Master timer

What is strange that interrupt from DMA related to ADC5 is coming but no data is in the buffer. In ADC1 everything is ok.

To be sure I have also deleated almost all unrelated things and only leaved ADC5, DMA and HRTIMER. The same thing happens.

Is there a way to go back to 1.2.0 package version and cube ide1.2.0 with existing project or i have to do it manually ? Or mayby wait for update?

UPDATE: With HAL on ADC5 it works. Is there something wrong with my code in LL and CMSIS ADC&DMA startup (and if yes, why ADC1 on LL&CMSIS works) ?

	  //ADC5
	  ADC5->CR &= ~ADC_CR_ADEN;	 // ensure ADC is off
	  ADC5->CR &= ~ADC_CR_ADCALDIF;  //single mode for calibration
	  ADC5 ->CR |= ADC_CR_ADCAL; //start the calibration of the ADC5
	  while (ADC5 ->CR & ADC_CR_ADCAL){}   //wait until calibration done
	  ADC5->CR |=ADC_CR_ADEN; //enable ADC5
          while(!(ADC5->ISR & ADC_ISR_ADRDY)); // wait until ADC is ready
 
 
	  // DMA1 CHANNEL 5
	  DMA1_Channel5->CPAR  = (uint32_t)(&(ADC5->DR)); // peripheral (source) address
	  DMA1_Channel5->CMAR = (uint32_t)&ADC5_TABLE; //MEMORY ADDRESS
	  DMA1_Channel5->CNDTR = ( uint16_t )ADC5_DATA_SIZE; //TRANSFER SIZE
	  DMA1_Channel5->CCR |= DMA_CCR_TCIE; //ENABLE TRANSFER COMPLETE INTERRUPT
	  DMA1_Channel5->CCR |= ( DMA_CCR_EN ); //CHANNEL ENABLE
 
 
	  ADC5->CR |=ADC_CR_ADSTART;

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
KoRba88
Associate III

Solved: Cube in MX_ADC5_init assigned ADC1 to these functions

 /* Disable ADC deep power down (enabled by default after reset state) */

 LL_ADC_DisableDeepPowerDown(ADC1);

 /* Enable ADC internal voltage regulator */

 LL_ADC_EnableInternalRegulator(ADC1);