Nucleo-G0B1RE Reset problem !!!!
I have recently bought Nucleo-G0B1RE Development board, When I power on, It worked perfectly I tested some programs on it and it worked very well. Then I ported my project on which I am working it executed sucessfully. But now I am facing weird problem, When I power on the nucleo board my none of the program is working !! In my project there is Monochrome graphics display used which is showing me the garbage, Even if I load the program from STM32Cube-IDE still it is not working and showing garbage on LCD. I doubt there is some reset problem on board. Please help me !!!
Thanks in advance