Skip to main content
Associate III
Jan 22, 2024 6:33 AM UTC
Solved

Is it possible to create a compile_commands.json file?

I work in a workspace but I use vim with clangd for editing my code. I am wondering if it is possible to create a compile_commands.json file and if so how. 
If the IDE uses cmake under the hood then it should be rather straightforward but I cannot understand how to proceed. 

see e.g. this:

https://cmake.org/cmake/help/latest/variable/CMAKE_EXPORT_COMPILE_COMMANDS.html

 

    ubaldotBest answer
    Associate III
    Jan 23, 2024 6:22 PM UTC

    I found an answer by myself, and it is YES.

    For those who may need it.

    Install a tool that can create a compile_commands.json from a makefile like compiledb or bear (in the following I will use compiledb)

    1) Go on Project->  Properties and change add the folder where compiledb is installed in PATH as shown below.

     

    ubaldot_0-1706033627690.png

     

    2) Go to Project -> Build Targets -> Create... Uncheck all the options and add the custom command you need for creating the compile_commands.json file in the Build commands. 

     

    ubaldot_1-1706033783099.png

    3) Select the newly created target on the left hand side of CubeIDE, right click and select Build Target.

    ubaldot_2-1706033967166.png


    4) Once your compile_commands.json is created, you have to move it in the upper folder (root of your project). 

    You may have some error related to cyclomatic-complexity, but to solve this is enough to open the compile_commands.json file and remove all the -fcyclomatic-complexity entries.

    OBS! I have just discovered this method, so take it with a grain of salt. 

    8 replies

    ubaldotAuthorBest answer
    Associate III
    Jan 23, 2024 6:22 PM UTC

    I found an answer by myself, and it is YES.

    For those who may need it.

    Install a tool that can create a compile_commands.json from a makefile like compiledb or bear (in the following I will use compiledb)

    1) Go on Project->  Properties and change add the folder where compiledb is installed in PATH as shown below.

     

    ubaldot_0-1706033627690.png

     

    2) Go to Project -> Build Targets -> Create... Uncheck all the options and add the custom command you need for creating the compile_commands.json file in the Build commands. 

     

    ubaldot_1-1706033783099.png

    3) Select the newly created target on the left hand side of CubeIDE, right click and select Build Target.

    ubaldot_2-1706033967166.png


    4) Once your compile_commands.json is created, you have to move it in the upper folder (root of your project). 

    You may have some error related to cyclomatic-complexity, but to solve this is enough to open the compile_commands.json file and remove all the -fcyclomatic-complexity entries.

    OBS! I have just discovered this method, so take it with a grain of salt. 

    Associate II
    Aug 14, 2024 10:14 AM UTC

    Thanks for this solution.
    I'm trying to set it up but I got an error: make: *** No rule to make target 'compile_command'. Stop.
    Is there anything to configure with the makefile?

    ubaldotAuthor
    Associate III
    Aug 15, 2024 7:58 AM UTC

    It was long ago, but looking at the screenshots I don't think you need to change the Makefile manually.
    Have you done the step 2) correctly? 

    Visitor II
    Aug 18, 2025 7:34 AM UTC

    Hi, 
    I am using STM32CubeIDE version 1.19.0 and I have right clicked my project, gone to properties, C/C++ Build, JSON Compiliation Database Generator. ticked the 2 boxes and away it went.

    average_joe_0-1755502481752.png

     

    Visitor II
    Aug 18, 2025 9:43 AM UTC

    Although, I am finging out it does not work in headless mode. As if your building in a docker.... bug or feature? 

    unsigned_char_array
    Lead III
    Apr 28, 2026 1:13 PM UTC

    @average_joe wrote:

    Although, I am finging out it does not work in headless mode. As if your building in a docker.... bug or feature? 


    It doesn't work in headless mode: https://community.st.com/t5/stm32cubeide-mcus/headless-linux-build-need-compile-commands-json-for-pclintplus/m-p/882423

    "Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."