Skip to main content
Senior
Sep 5, 2024 2:13 PM UTC
Solved

How to Use a Variable in SRAM to Communicate between Bootloader and Application

Hi,

I have a bootloader for my application, at the moment they exchange their working status by flash write. I think a better way is to declare a variable in RAM with the same address in both bootloader and application. Someone mentioned, in a post, that the linker script could be used for this, but didn't give an example.

Anybody could do me a favour and show me an example ? Thanks.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 9, 2024 9:01 AM UTC

Set the memory origin at 0x20000004 and your common variable at 0x20000000.

 

_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */

/* Memories definition */
MEMORY
{
...
RAM (xrw) : ORIGIN = 0x20000004, LENGTH = 49152 /* 48K - 4 bytes*/
...
}

 

#define COMMON_VAR_ADDRESS 0x20000000 /* Define a common RAM address */

uint32_t* common_var = (uint32_t*)COMMON_VAR_ADDRESS; /* Declare a pointer at that address */
*common_var = y; /* access to that address */
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

11 replies

mƎALLEm
ST Technical Moderator
Sep 5, 2024 2:18 PM UTC

@Chao wrote:

Someone mentioned, in a post, that the linker script could be used for this, but didn't give an example.

Anybody could do me a favour and show me an example ? Thanks.


Using __attribute . See this link: https://www.openstm32.org/Using%2BCCM%2BMemory

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
MM..1
Super User
Sep 5, 2024 2:40 PM UTC

Maybe we require info how working status you mean... And most simple method to share is move start RAM +somethink for example 0x20000020 and use direct pointers to 0-1F arrea. 

mƎALLEm
ST Technical Moderator
Sep 5, 2024 2:54 PM UTC

Yes @MM..1 it could be also a solution.

 

 

#define COMMON_VAR_ADDRESS 0x2000XXXX /* Define a common RAM address */

uint32_t* common_var = (uint32_t*)COMMON_VAR_ADDRESS; /* Declare a pointer at that address */
*common_var = y; /* access to that address */

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Sep 9, 2024 9:01 AM UTC

Set the memory origin at 0x20000004 and your common variable at 0x20000000.

 

_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of "RAM" Ram type memory */

/* Memories definition */
MEMORY
{
...
RAM (xrw) : ORIGIN = 0x20000004, LENGTH = 49152 /* 48K - 4 bytes*/
...
}

 

#define COMMON_VAR_ADDRESS 0x20000000 /* Define a common RAM address */

uint32_t* common_var = (uint32_t*)COMMON_VAR_ADDRESS; /* Declare a pointer at that address */
*common_var = y; /* access to that address */
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.