Skip to main content
Senior
July 23, 2024
Solved

How to see which project the currently opened file belongs to

  • July 23, 2024
  • 2 replies
  • 1388 views

Hi,

when you have multiple projects loaded in the IDE (pane on the left hand side) and also multiple files opened (each from different projects) how do you know which one belongs to which project?

 

AND... how can you tell which project is the active one being compiled?

 

In pretty much every other IDE environment when you open a file it automatically highlights it name in the tree on the left side. But not on the CubeIDE...

 

For example if you have two main.c open you have no idea which one belongs to which project currently loaded in the IDE...

 

Thank you :)

This topic has been closed for replies.
Best answer by TDK

When your cursor is in the file, the title bar will show which project the current file belongs to, along with its path.

Your cursor also selects which is the active project, by having your cursor within a file of that project. That's the project that will get built if you do Project -> Build Project.

2 replies

Karl Yamashita
Principal
July 23, 2024

Just hover over the file tab. Not sure if it's a Eclipse thing, but even CCS does the same as STMCubeIDE.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
TDK
TDKBest answer
July 23, 2024

When your cursor is in the file, the title bar will show which project the current file belongs to, along with its path.

Your cursor also selects which is the active project, by having your cursor within a file of that project. That's the project that will get built if you do Project -> Build Project.

"If you feel a post has answered your question, please click ""Accept as Solution""."