Skip to main content
Associate
May 27, 2024
Solved

HAL_Delay() --> SysTick_Handler never be called

  • May 27, 2024
  • 6 replies
  • 2088 views

Hi all,

Version: 1.15.1

MCU : g473

Before investigate deeply on my own I wonder whether if anyone have faced the same problem with Interrupt table in general ...

I placed a breakpoint there :

void SysTick_Handler(void)

{

/* USER CODE BEGIN SysTick_IRQn 0 */

 

/* USER CODE END SysTick_IRQn 0 */

HAL_IncTick();

/* USER CODE BEGIN SysTick_IRQn 1 */

 

/* USER CODE END SysTick_IRQn 1 */

}

and surprisingly the code is never executed !

Best regards,

 

 

 

    This topic has been closed for replies.
    Best answer by Sarra.S

    Hello @bibah, 

    Uncommenting the "define USER_VECT_TAB_ADDRESS" allows for the relocation of the vector table, which can be necessary for certain applications (that's why I asked about the bootloader) or when the application needs to be located at a specific address in memory, that's why maybe some details are required on your application...

    In previous STM32CubeMX versions, the line #define USER_VECT_TAB_ADDRESS was uncommented by default, which would automatically relocate the vector table, but in later versions, for more flexibility,  you have the choice to uncomment it if you need to.

    6 replies

    ST Employee
    May 27, 2024

    Hello @bibah, 

    Have you used CubeMX to generate the code? if yes, what's the version? 

    Also, maybe provide some context, are you using a bootloader, or have remapped the vector table?

    The SysTick timer needs to be initialized before it can trigger interrupts, I assume you did that

    Maybe verify systick interrupt priority? and ensure that global interrupt is enabled

     

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    bibahAuthor
    Associate
    May 28, 2024

    Hi Sarra,

     

    STM32CubeMX - STM32 Device Configuration Tool

    Version: 6.11.1-RC2

    Build: 20240411-0753 (UTC)

     

    No BootLoader and no remapped the Vector Table

     

    Early in the code generated by CubeMX

    • HAL_Init();
    • SystemClock_Config();
    • MX_NVIC_Init()
    • ....

    And finally I found a solution detailed here :

     I uncommented /*#define USER_VECT_TAB_ADDRESS*/ in system_stm32g4xx.c so it lay on Flash now

    /************************* Miscellaneous Configuration ************************/

    /* Note: Following vector table addresses must be defined in line with linker

    configuration. */

    /*!< Uncomment the following line if you need to relocate the vector table

    anywhere in Flash or Sram, else the vector table is kept at the automatic

    remap of boot address selected */

    #define USER_VECT_TAB_ADDRESS

     

    #if defined(USER_VECT_TAB_ADDRESS)

    /*!< Uncomment the following line if you need to relocate your vector Table

    in Sram else user remap will be done in Flash. */

    /* #define VECT_TAB_SRAM */

    #if defined(VECT_TAB_SRAM)

    #define VECT_TAB_BASE_ADDRESS SRAM_BASE /*!< Vector Table base address field.

    This value must be a multiple of 0x200. */

    #define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.

    This value must be a multiple of 0x200. */

    #else

    #define VECT_TAB_BASE_ADDRESS FLASH_BASE /*!< Vector Table base address field.

    This value must be a multiple of 0x200. */

    #define VECT_TAB_OFFSET 0x00000000U /*!< Vector Table base offset field.

    This value must be a multiple of 0x200. */

    #endif /* VECT_TAB_SRAM */

    #endif /* USER_VECT_TAB_ADDRESS */

    /******************************************************************************/

     

    My question :

     

    Is it a normal situation the Vector Table will not be generated by default ?

     

    Best Regards, H

    Sarra.SBest answer
    ST Employee
    June 7, 2024

    Hello @bibah, 

    Uncommenting the "define USER_VECT_TAB_ADDRESS" allows for the relocation of the vector table, which can be necessary for certain applications (that's why I asked about the bootloader) or when the application needs to be located at a specific address in memory, that's why maybe some details are required on your application...

    In previous STM32CubeMX versions, the line #define USER_VECT_TAB_ADDRESS was uncommented by default, which would automatically relocate the vector table, but in later versions, for more flexibility,  you have the choice to uncomment it if you need to.

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    bibahAuthor
    Associate
    June 7, 2024

    Ok Sarra,

    Got it ! Thanks. May be you should include this feature in CubeMX ... no ?

    Habib