Skip to main content
DKuro.1
Associate III
May 6, 2020
Solved

DMA IRQ Handler is called twice for ADC

  • May 6, 2020
  • 2 replies
  • 1489 views

Hi,

I am using 3 ADC modules triggered with TIM3 to start in the same time.

I read the result in the DMAx_Channely_IRQHandler function and for debug only I do a toggle in a GPIO.

I have 3 DMAx_Channely_IRQHandler functions , one for each ADC with DMA and 3 output pint that I toggle

All of the outputs are showing me that the DMAx_Channely_IRQHandler function is called twice.

I am using STM32G474 and STM32CubeIDE, with HAL.

Why is this happening and how can I fix it?

Thanks!!

 HAL_ADC_Start_DMA(&hadc1, (uint32_t *)data_ADC_1, N_CH);
 HAL_ADC_Start_DMA(&hadc2, (uint32_t *)data_ADC_2, N_CH);
 HAL_ADC_Start_DMA(&hadc3, (uint32_t *)data_ADC_3, N_CH);
 
---------------
 
 
static void MX_DMA_Init(void) 
{
 
 /* DMA controller clock enable */
 __HAL_RCC_DMAMUX1_CLK_ENABLE();
 __HAL_RCC_DMA2_CLK_ENABLE();
 __HAL_RCC_DMA1_CLK_ENABLE();
 
 /* DMA interrupt init */
 /* DMA1_Channel2_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel2_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel2_IRQn);
 /* DMA1_Channel3_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel3_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel3_IRQn);
 /* DMA2_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA2_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA2_Channel1_IRQn);
 
} 
 
 
-------------
 
static void MX_ADC1_Init(void)
{
 
 /* USER CODE BEGIN ADC1_Init 0 */
 
 /* USER CODE END ADC1_Init 0 */
 
 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};
 
 /* USER CODE BEGIN ADC1_Init 1 */
 
 /* USER CODE END ADC1_Init 1 */
 /** Common config 
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.GainCompensation = 0;
 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 3;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T3_TRGO;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure the ADC multi-mode 
 */
 multimode.Mode = ADC_MODE_INDEPENDENT;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel 
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel 
 */
 sConfig.Rank = ADC_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel 
 */
 sConfig.Rank = ADC_REGULAR_RANK_3;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */
 
 /* USER CODE END ADC1_Init 2 */
 
}
 
 
-----------
 
void DMA1_Channel2_IRQHandler(void)
{
 /* USER CODE BEGIN DMA1_Channel2_IRQn 0 */
 
 /* USER CODE END DMA1_Channel2_IRQn 0 */
 HAL_DMA_IRQHandler(&hdma_adc2);
 /* USER CODE BEGIN DMA1_Channel2_IRQn 1 */
 adc22_cnt++;
 data_adc2 = data_ADC_2[0];
 HAL_GPIO_TogglePin(END_CONV_2_GPIO_Port, END_CONV_2_Pin);
 /* USER CODE END DMA1_Channel2_IRQn 1 */
}
 
 

This topic has been closed for replies.
Best answer by Tesla DeLorean

Perhaps it triggers both HT and TC interrupts, perhaps you should quantify the source before toggling the pin, or do it in the callbacks?

2 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
May 6, 2020

Perhaps it triggers both HT and TC interrupts, perhaps you should quantify the source before toggling the pin, or do it in the callbacks?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DKuro.1
DKuro.1Author
Associate III
May 6, 2020

Thanks clive!!!

It was that the HT and TC interrupts enabled

:)