Skip to main content
Associate II
Jan 26, 2025 9:49 AM UTC
Question

Cmsis-DAP debugger in STM32CubeIDE

Hello, i have a DapLink debugger and wanted to use it with stm32, i also am pretty new to stm32, so don't be mad when i mess up some terms. I don't want to buy an STLink yet since i wanna see if i am going to like stm32 debugging/programming. Some context:MCU:STM32H723ZGT6, debugger: DapLink Mini, OS:Ubuntu desktop 24.10.Also, yes i know that this board is overkill but i thought, go big or go home, if i am gonna try stm32 i better make it count.

This topic has been closed for replies.

40 replies

Visitor II
Apr 22, 2025 8:37 PM UTC

I found the steps to upload and debug with a cheap daplink. See my post on imgur (https://imgur.com/a/how-to-use-daplink-cmsis-dap-with-stm32cubeide-OrpcsvX) - or I'll copy paste its contents below:

---

How to use daplink (cmsis-dap) with STM32CubeIDE


ckocagil_5-1745353772389.png
You can use a cheap and standard cmsis-dap device to flash and debug stm32 projects within the cube ide. Let's start with a fresh project.
 
 
 
 
 
ckocagil_6-1745353942962.png
I hook up the dap with 4 wires (vcc, gnd, swdio, swclk) and no reset wire. For this to work without having to constantly manually reset the device, I go to SYS and change Debug mode to Serial Wire. Save and generate code. Build.
 
 
 
 
 
ckocagil_8-1745353989610.png
Next, we create a file daplink.cfg in the project root. The file should contain:
source [find interface/cmsis-dap.cfg]
adapter speed 1000
transport select swd
source [find target/stm32f1x.cfg]
reset_config none
 
 
 
 
 
ckocagil_10-1745354083720.png
Now go to Run -> Debug Configurations and create a debug config. Make sure the C/C++ Application field contains our elf file.
 
 
 
 
 
ckocagil_3-1745353712160.png
The crucial part: on the Debugger tab, we change the probe to OpenOCD, select User Defined script, and use our daplink.cfg.
 
Click Apply to save our debug config and that should be all. You're now ready to run or debug your code.
 
QUIRKS: For some reason, ST's openocd scripts leave the mcu paused after detaching the dap. This means every time you Run your code or detach a Debug session, your mcu will need a manual reset.
 
My workaround for this is to add the following line at the end of daplink.cfg:
 
lappend pre_shutdown_commands { resume }

 

AScha.3
Super User
Apr 27, 2025 10:04 AM UTC

Hi, @ckocagil ,

i tried with daplink.cfg script to connect an old blue-pill (with STM32F103C6 cpu) and yes, its working fine !

Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : CMSIS-DAP: SWD supported
Info : CMSIS-DAP: Atomic commands supported
Info : CMSIS-DAP: Test domain timer supported
Info : CMSIS-DAP: FW Version = 2.1.0
Info : CMSIS-DAP: Serial# = 070000011a5a5bb6000000000001ceeca5a5a5a597969908
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : clock speed 4000 kHz
Info : SWD DPIDR 0x1ba01477
Info : [STM32F103C6Tx.cpu] Cortex-M3 r1p1 processor detected
Info : [STM32F103C6Tx.cpu] target has 6 breakpoints, 4 watchpoints
Info : [STM32F103C6Tx.cpu] Examination succeed
Info : starting gdb server for STM32F103C6Tx.cpu on 3333
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : device id = 0x10006412
Info : flash size = 32 KiB
Warn : GDB connection 1 on target STM32F103C6Tx.cpu not halted
undefined debug reason 8 (UNDEFINED) - target needs reset
Info : accepting 'gdb' connection on tcp/3333
Warn : GDB connection 2 on target STM32F103C6Tx.cpu not halted
undefined debug reason 8 (UNDEFINED) - target needs reset
[STM32F103C6Tx.cpu] halted due to breakpoint, current mode: Thread 
xPSR: 0x01000000 pc: 0x080004a4 msp: 0x20002800

So i can use my -until now useless- cmsis-dap debug probe also .

Great !

(But usually using st-link V2 or V3  , its just nice, to have a working alternative debug probe. )

If you feel a post has answered your question, please click on " Best Answer ".
Andrew Neil
Super User
Apr 30, 2025 6:57 AM UTC



@atleasttwocharacterslong wrote:

Why is the topic you guys split it into showing up as read only?


Explained here: https://community.st.com/t5/others-stm32-mcus-related/blackmagic-debug-probe-in-stm32cubeide/m-p/797963/highlight/true#M6548

 


@atleasttwocharacterslong wrote:

 i do not want to buy an st-link because i want one tool for all cortex-m devices, and not one tool for ST's STM32, one for TI's msp or whatever and so on.


That's fair enough - but it's also fair that ST's resources are dedicated to supporting ST's own products.

If you had a J-Link, you would expect Segger to support it - rather than ST.

You need to weigh the advantage of having a single probe against the "cost" of the loss of specific vendor support.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.