Skip to main content
Associate
Jan 12, 2026 3:07 PM UTC
Solved

Breakpoint installation failure unmatched quote

Hello. I am currently working on a NUCLEO-L152RE project in the latest version of the CubeIDE. I am running into an error where I can not install break points due to an "unmatched quote". I have tried the common fixes (New work space) for this that I could find online and it hasn't resolved it. I also ran fresh installs of the programs and encountered the same issue. Has anyone else encountered this problem? I have included a screenshot below for reference. 

 

ddwertz_0-1768230405538.png

 

Andrew Neil
Andrew NeilBest answer
Super User
Jan 12, 2026 4:38 PM UTC

@ddwertz wrote:

This is the file path shown in the IDE

ddwertz_1-1768235427673.png


I added a PS to my previous post - it looks like the single quote might also upset things...

Check also what "OneDrive - Personal" actually translates to ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

12 replies

Andrew Neil
Super User
Jan 12, 2026 3:21 PM UTC

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results

 

In particular, what version of Cube are you using, and on what platform?

Please describe in detail the steps you take to get to this error.

 


@ddwertz wrote:

I am currently working on a NUCLEO-L152RE project


Is this a project you've created yourself, an ST example, or something else?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ddwertzAuthor
Associate
Jan 12, 2026 3:34 PM UTC

I am using the 2.0.0 Build of both the IDE and MX software. I used the MX file to generate the initial code and then added some generic lines (incrementing an integer). This is the second project I have created using the MX and they both have the same problem. I am running the software on a Windows 11 set up. As far as I can tell everything functions properly except for the breakpoints.

TDK
Jan 12, 2026 3:22 PM UTC

Does the project build and run successfully?

Maybe there is an unmatched quote in the file or a file it includes. It's unlikely to be making things up--this is parsed, not AI.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ddwertzAuthor
Associate
Jan 12, 2026 3:38 PM UTC

The project builds and runs as intended. The breakpoint is to be inserted as part of a lab exercise to show functionality.  When I manually stop/start the program it functions as intended, it just won't allow me to insert a breakpoint. As far as the included files I generated it in MX (ver 2.0.0).

Andrew Neil
Super User
Jan 12, 2026 4:53 PM UTC

you're welcome.

As noted, this is a very common cause of weird problems like this - so it's always best to avoid spaces and other special characters in file & folder names used for software development.

 

Please pass this onto your TA and course instructor - it's something they should be warning students about!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.