Solved
2D-FFT rfft and cfft functions
I have a 2D array input buffer. so, what is the correct way to implement the rfft and cfft functions?
float fftIn[16][512] is my input. So, I applied for a loop like below:
arm_rfft_fast_init_f32(&fftHandler, 512);
for(int d =0; d<16; d++){
arm_rfft_fast_f32(&fftHandler, &fftIn[d], &fftOut[d], 0);
}
Is this the correct way?
Since the fftout will be complex no. I have taken cfft along the column(by rearranging the 2d array in certain way) like below:
Here input is like fft2In[256][32]
for(int e = 0; e<256; e++){
arm_cfft_f32(&arm_cfft_sR_f32_len16, &fft2In[e], 0, 0);
}
arm_cfft_f32(&arm_cfft_sR_f32_len16, &fft2In[e], 0, 0);
}
Again is the correct way to implement? I am getting some output but I don't have a way to verify the result as of now.
Please help me with this?