Skip to main content
Semer CHERNI
ST Employee
July 10, 2023
Question

STM32CubeIDE 1.13.0 released

STM32CubeIDE 1.13.0 was released today on st.com as well as an in-tool update patch.

  • What is new in 1.13.0?
    • Added the support for new microcontrollers in the STM32U5 series
    • Added the support for new microcontrollers in the STM32WBA series
    • Added the support for two new boards related to the STM32U5 series: STM32U5G9J-DK1 and STM32U5G9J-DK2
    • Added the support for one new board related to the STM32L4+ series: STEVAL-SMARTAG2
    • Added the user authentication interface to permit package download
    • Updated to Eclipse® 2023-03
    • Updated to GCC 11 support by default
    • Added CMake project support
  • Updated debug:
    • Changed values highlighted in yellow in the SFRs view
    • Debug authentication for STM32H5 products
    • Support for programming using multiple external loaders with OpenOCD
  • Updated for microprocessors:
    • Support for the latest release 5.0.0 of OpenSTLinux
    • Addition of the TCP console for semihosting output
  • Main fixed issues
    • 109036 [UC5-REGENERATE][CubeIDE][Examples]Build failed when changing some configurations of LoRaWAN_End_Node example
    • 131635 Add option to highlight when a live variable changes its value
    • 143369 STM32CubeMX Linker script generation problem
  • Known issues fixed and problems and limitations
    • Please refer to the wiki.
  • Where do I obtain STM32CubeIDE 1.13.0?
    This topic has been closed for replies.

    12 replies

    Graduate II
    July 11, 2023

    Hello

    This latest version 1.13.0 seems to give error to sysmem.c like this:

    JTP1_1-1689098566183.png

    CubeIDE 1.12.0 compiles the same project without any problem.

    Projects are generated from TouchGFX template (4.21.4 or 4.22.0) and then imported and compiled in CubeIDE. I know that this can be fixed by changing caddr_t to void or including <sys/types.h> to sysmem.c

    But what is the reason for this different behavior in CubeIDE 1.12.0 and 1.13.0 , new GCC version ? I'm afraid this will cause more issues to people how is trying to study TGFX.

    br. J.T

     

     

    Semer CHERNI
    ST Employee
    July 12, 2023

    Hello @JTP1 

    Yes indeed the GCC version was upgraded from GCC10 to GCC11 with the STM32CubeIDE 1.13.0.

    You are right with the solution you have proposed of changing the caddr_t to void* or include the <sys/types.h> to sysmem.c.

    With this been said, I will raise the issue internally to review it and provide a permanent solution.

    KR,

    Semer.

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    padawan
    Senior II
    July 12, 2023

    ID 

    139768After programming a device CubeIDE opens every time a new tab with startup file and give focus on that tab.

    is not fixed!

     

    The new tab will also be opened when entering and leaving the debug mode!

    So after "Debug" you have 2 more tabs open!

    Andrei Chichak
    Lead
    July 12, 2023

    Please take a look at:

    https://community.st.com/t5/embedded-software-mcus/error-after-calling-printf/td-p/574044

    I've restored back to 1.12.1 to continue working.

    Visitor II
    July 16, 2023

    I have noticed that the new release starts loading the macOS too much. I have at least 50% CPU load by Chrome Helper GPU (and render the process as well) that runs CubeIDE. I reinstalled ide with a fresh installation and got the same result.

    PHolt.1
    Senior
    July 16, 2023

    The GCC v11 tools (Cube v1.13) break a few things.

    One is the has no explicit encoding set warning mentioned here
    https://community.st.com/t5/stm32cubeide-mcu/has-no-explicit-encoding-set-warning/td-p/574835
    Despite extensive googling I cannot find a fix for it. The various fixes for eclipse do not work, and neither does the one under project / properties / resource

    PHolt1_0-1689538045194.png

     

    Another is detailed here
    https://www.eevblog.com/forum/programming/stm32f4-gcc-v12-to-v13-some-weird-error-messages/

    I think some compiler checking options have changed.

     

    PHolt.1
    Senior
    July 17, 2023

    This has been fixed - see eevblog link above.

     

    JojoS
    Associate III
    July 18, 2023

    After upgrading from 1.12 to 1.13, the debugger stops suddenly after hitting a breakpoint. Also stops after a few steps. The debugger console does not show exceptions.

    edit:
    I've reverted now also to 1.12.1, 1.13.0 is unusable for me. The debugger stops with nothing more than 'client has disconnected', same code with 1.12 no problem. I had cleaned and rebuild the project.
    After rebuilding, 1.13 pops up an error, but build is ok.

    build-fehler.jpg

    1.13 adds some template code that produces duplicate symbols. It also adds MPU_initialize which produces unused warning.
    Such simple things are not discovered by testing a new release?

    PScal
    Associate II
    July 19, 2023

    After installing STM32CubeIDE 1.13.0 I have no menu bar any further. I tried to configure menu bar visibility for perspectives, which had no effect. I also tried to reinstall STM32CubeIDE 1.13.0 but still no menu bar. 

    I am running windows 11 and having STM32CubeIDE 1.12.1 and 1.13.0 installed in two separate folders. 

    best regards 

    PScal

    DavidAlfa
    Senior II
    July 28, 2023

    I always had issues when upgrading.

    Best way  is to uninstall the current IDE and install the new one.

    If still having issues, delete the .metadata folder in the workspace.

    Andrei Chichak
    Lead
    July 28, 2023

    Upgrading on a macOS box just works. Downgrading was easy too, just get time machine to take it back to before the update.

    I find it weird that after 40 years, Microsoft still treats backups as second class citizens.