Skip to main content
JStei.6
Associate II
Aug 17, 2023 7:06 PM UTC
Question

STM32Cube IDE "Run" works, "Debug" doesn´t

Hello everyone,

I have a problem with my STM32f746g_Disco. When I started a project, I could hit the "Debug" button and everything worked fine.

Now it uploads everything and the Screen just shows a static noise (like on an old TV). When I use the "Run" button next to the "Debug" button, everything works as expected. So there is no code Error.

But now I cannot use the debug function, wich is essential for me.

I could not find any differences between the "debug Configurations" and "run configurations". Is there another place I could look for differences?

 

 

When Using "Debug" the console is giving me the following lines:

	STMicroelectronics ST-LINK GDB server. Version 7.3.0	
Copyright (c) 2023, STMicroelectronics. All rights reserved.	
Starting server with the following options:	
 Persistent Mode : Disabled	
 Logging Level : 1	
 Listen Port Number : 61234	
 Status Refresh Delay : 15s	
 Verbose Mode : Disabled	
 SWD Debug : Enabled	
 InitWhile : Enabled	
Waiting for debugger connection...	
Debugger connected	
Waiting for debugger connection...	
Debugger connected	
Waiting for debugger connection...	
 -------------------------------------------------------------------	
 STM32CubeProgrammer v2.13.0 	
 -------------------------------------------------------------------	
Log output file: C:\Users\Model\AppData\Local\Temp\STM32CubeProgrammer_a24180.log	
ST-LINK SN : 066FFF534956866687013736	
ST-LINK FW : V2J41M27	
Board : 32F746GDISCOVERY	
Voltage : 3.24V	
SWD freq : 4000 KHz	
Connect mode: Under Reset	
Reset mode : Hardware reset	
Device ID : 0x449	
Revision ID : Rev Z	
Device name : STM32F74x/STM32F75x	
Flash size : 1 MBytes	
Device type : MCU	
Device CPU : Cortex-M7	
BL Version : 0x90	
Debug in Low Power mode enabled	
Memory Programming ...	
Opening and parsing file: ST-LINK_GDB_server_a24180.srec	
 File : ST-LINK_GDB_server_a24180.srec	
 Size : 599.43 KB 	
 Address : 0x08000000 	
Erasing memory corresponding to segment 0:	
Erasing internal memory sectors [0 6]	
Download in Progress:	
File download complete	
Time elapsed during download operation: 00:00:10.570	
Verifying ...	
Download verified successfully

When using "run" I get the following:

STMicroelectronics ST-LINK GDB server. Version 7.3.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
 Persistent Mode : Disabled
 Logging Level : 1
 Listen Port Number : 61234
 Status Refresh Delay : 15s
 Verbose Mode : Disabled
 SWD Debug : Enabled
 InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.13.0 
 -------------------------------------------------------------------
Log output file: C:\Users\Model\AppData\Local\Temp\STM32CubeProgrammer_a06584.log
ST-LINK SN : 066FFF534956866687013736
ST-LINK FW : V2J41M27
Board : 32F746GDISCOVERY
Voltage : 3.24V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x449
Revision ID : Rev Z
Device name : STM32F74x/STM32F75x
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x90
Debug in Low Power mode enabled
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a06584.srec
 File : ST-LINK_GDB_server_a06584.srec
 Size : 599.43 KB 
 Address : 0x08000000 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 6]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:10.765
Verifying ...
Download verified successfully 
Shutting down...
Exit.

I don´t see any differences there.

After using the "debug" command, I always press "resume" to start the programm. Is anything wrong with that?

 

Thanks for your help!

    This topic has been closed for replies.

    6 replies

    RhSilicon
    Lead
    Aug 17, 2023 8:38 PM UTC

    I don't know if it can help in your case, but I found these videos about advanced debugging:

    STM32CubeIDE Advanced Debug Features
    https://youtube.com/playlist?list=PLnMKNibPkDnEDEsV7IBXNvg7oNn3MfRd6

    TDK
    Aug 17, 2023 9:52 PM UTC

    In Debug configurations, uncheck the "set breakpoint on main" box. This will let you launch it without having to "resume" when it hits the breakpoint at main, which may be causing the issue.

    You can also set "Download: False" which will cause it not to update the flash before it runs the program. To debug in this mode, hit "Run" to upload the file, then hit "Debug" and it will attach to the process wherever it happens to be at. I don't think there is any upset in program flow, but there may be something minor.

    TDK_1-1692309142695.png

     

    "If you feel a post has answered your question, please click ""Accept as Solution""."
    Rim LANDOLSI
    ST Employee
    Aug 18, 2023 1:14 PM UTC

    Hello @JStei.6 ,

    Could you, please, share a screenshot of the debug configuration. You could activate the gdb-server log in the debug configuration. It would be , also, helpful to post the gdb-server log and the .launch file that's in the root of your project .

    RimLANDOLSI_0-1692364425462.png

    Thanks,

    Rim

    JStei.6
    JStei.6Author
    Associate II
    Aug 19, 2023 3:34 PM UTC

    I have tried a bit here and there. Turning off "Download" as suggested by TDK didn´t do anything. But I looked into other projects that still debug correctly, and the external loader was not configured correctly. But it is still behaving weired. 

    "Run" still works perfectly fine, and programming it with the "STM32CubeProgrammer" also works fine, but when I try "Debug" it downloads everything, but when I hit the "Resume" button, it shows the startup screen of the last program that was loaded to it (with a few of missing pixels) as if the starting occures at a wrong memory spot. Now I can press the reset button, and the correct program starts.

     

    Here are my screenshots of the debug config:

    SamPlay_debug_2.pngSamPlay_Debug_1.png

     

    I could not upload the .launch file because the file format is not supported, and the gdb server log is too big to be uploaded. So I put it into my onedrive cloud an I have generated the following link:

     https://1drv.ms/f/s!AjN2hZR42EKhiPZ-X5K2Wf9nbSoTNQ?e=bpnIMF

     

    Thank you!

    Rim LANDOLSI
    ST Employee
    Aug 21, 2023 3:18 PM UTC

    It seems that you are working with an old STM32CubeIDE version. Could, please, you try the project with newer version.

    JStei.6
    JStei.6Author
    Associate II
    Aug 22, 2023 2:47 PM UTC

    I have now updated to 1.13.1 but nothing changed.

    I have tried different things now and saved the gdb server logs.

    The two logs where I have unchecked the "download" option are small enough to be uploaded here.

    The behaviour is the same. Run works, debug just gives static noise. (The programm has been downloaded with "run". Then the the "download" checkbus has been unchecked, then the two server logs were created.

    everything else is on the cloud (same Link from my last post).

     

    Another thing I noticed is that when the problem occurs, CubeIde alway higlights the "HardFault_Handler" in "stm32f7xx_it.c" So something while debugging causes this hardfault. "Run" does not do that.