Skip to main content
Associate
August 29, 2023
Solved

Microcontroller is not sending data over serial line, but does appear to be collecting it

  • August 29, 2023
  • 1 reply
  • 1236 views

I added in another printf statement just to make sure it was working. In the putty terminal I was able to see "Hello world", but not the actual data I needed to see: printf("Time: %lu ms, Input Voltage: %.2f V\n", HAL_GetTick() - start_time, input_voltage); I believe the microcontroller is not sending data over serial line, but does appear to be collecting it, however there could be another issue. I am using a NUCLEO-F767ZI microcontroller, and using STM32CubeIDE.

This is my code:

#include <stdio.h>

#include <stdlib.h>

#include "stm32f7xx_hal.h"

 

/* Define UART handle */

UART_HandleTypeDef huart3;

 

ADC_HandleTypeDef hadc; // Declare 'hadc' here

 

void Error_Handler(void) { while (1); }

void SystemClock_Config(void) { /* Configure system clock here */ }

 

/* Initialize UART */

void init_uart(void) {

huart3.Instance = USART3;

huart3.Init.BaudRate = 9600; // Baud rate: 9600 bps

huart3.Init.WordLength = UART_WORDLENGTH_8B;

huart3.Init.StopBits = UART_STOPBITS_1; // Stop bits: 1

huart3.Init.Parity = UART_PARITY_NONE; // Parity: None

huart3.Init.Mode = UART_MODE_TX_RX;

huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE;

huart3.Init.OverSampling = UART_OVERSAMPLING_16;

HAL_UART_Init(&huart3);

}

 

/* Custom implementation of _write for printf redirection */

int _write(int file, char *ptr, int len) {

HAL_UART_Transmit(&huart3, (uint8_t*)ptr, len, HAL_MAX_DELAY);

return len;

}

 

void init_gpio(void) {

// GPIO initialization code

}

 

void init_timer(void) {

// Timer initialization code

}

 

void init_adc(void) {

// ADC initialization code

}

 

int main(void) {

HAL_Init();

SystemClock_Config();

init_uart();

init_gpio();

init_timer();

init_adc();

 

uint32_t start_time = 0;

float input_voltage = 0.0f;

 

while (1) {

printf("Hello World\n");

 

start_time = HAL_GetTick(); // Start time for capturing voltage data

 

while (HAL_GetTick() - start_time < 5000000) // Capture data for 5 seconds

{

// Read data from ADC and process if needed

// (similar to previous ADC reading code)

 

// Print voltage and time

HAL_ADC_Start(&hadc); // Declare 'hadc' here

HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY);

 

uint32_t adc_value = HAL_ADC_GetValue(&hadc);

input_voltage = (float)adc_value / 4095.0f * 3.3f;

 

HAL_ADC_Stop(&hadc);

 

printf("Time: %lu ms, Input Voltage: %.2f V\n", HAL_GetTick() - start_time, input_voltage);

 

// No fflush(stdout) here

 

HAL_Delay(1); // Delay between voltage measurements

}

 

printf("Measurement done\n"); // Output to indicate end of measurement

}

}

 

This topic has been closed for replies.
Best answer by TDK

> ADC_HandleTypeDef hadc;

You never initialize this. No doubt the first ADC call fails. Look at ADC examples. Cube generates this code for you, how did it get lost?

Step through, monitor return value from HAL functions to verify success or failure.

1 reply

TDK
TDKBest answer
August 29, 2023

> ADC_HandleTypeDef hadc;

You never initialize this. No doubt the first ADC call fails. Look at ADC examples. Cube generates this code for you, how did it get lost?

Step through, monitor return value from HAL functions to verify success or failure.

"If you feel a post has answered your question, please click ""Accept as Solution""."