FreeRTOS: Only one of two tasks are occurring
- 2 replies
- 5847 views
Hello,
I am utilizing a FreeRTOS system on the STM32H725AGI6 in my software with two purposes:
- Run a task that handles the TouchGFX process to operate an LCD display
- Run a task that handles a BLE process (Which utilizes the
BlueNRG-M0A)
I have tested both processes separately and both work as I intend them to.
I created the two tasks with the FreeRTOS system and observed that:
- If I comment out the creation of the TouchGFX task in the main.c, the BLE portion works as intended
- If I comment out the creation of the BLE Task, in the main.c, the TouchGFX portion works as intended
- If I run both tasks at the same time, the TouchGFX portion works as intended, the BLE initialization code is run, but the repeated process (MX_BlueNRG_MS_Process()) is never called.
I've included the task initialization and process for both below. Additionally, I've attached my CubeMX configuration for the FreeRTOS system.
I have tried to do the following:
- Increase the cheap size to 35000
- Add osDelay(1) into the TouchGFX Task
- Remove the BLE Task and have the process called as part of a timer interrupt instead
None of the above solutions solved the problem.
I am unfamiliar with FreeRTOS on a deep level, but I suspect it is related to memory management and/or the priority system of the tasks, but I am unsure of how to prove this and diagnose this problem. The reason I suspect it's a memory issue though is that I'm running at 94.61% of Internal RAM usage. I allocate the entire TouchGFX task and 480x272, RGB565 array in the Internal RAM, which is why it's so heavily used.

I attached my BLE portion of the code so that the MX_BlueNRG_MS_Init() and MX_BLUENRG_MS_Process() can be reviewed to try and get a better understanding.
Can someone please help me get some insight on this issue?
void BLE_Task(void *argument)
{
/* USER CODE BEGIN BLE_Task */
MX_BlueNRG_MS_Init();
/* Infinite loop */
for(;;)
{
osDelay(1);
MX_BlueNRG_MS_Process();
}
/* USER CODE END BLE_Task */
}
void TouchGFXHAL::taskEntry()
{
enableLCDControllerInterrupt();
enableInterrupts();
OSWrappers::waitForVSync();
backPorchExited();
/* Assert display enable LCD_DISP_CTRL pin */
//HAL_GPIO_WritePin(GPIOA, GPIO_PIN_2, GPIO_PIN_SET);
/* Assert back light LCD_BL_CTRL pin */
//HAL_GPIO_WritePin(GPIOA, GPIO_PIN_1, GPIO_PIN_SET);
for (;;)
{
//OSWrappers::taskDelay(1);
OSWrappers::waitForVSync();
backPorchExited();
}
}