Skip to main content
Associate
February 11, 2025
Solved

N6 VS Code launch.json for debugging

  • February 11, 2025
  • 7 replies
  • 4096 views

I'm having some difficulty getting debugging working in VSCode for the N6 series.  Does anyone have a sample one that actually works?  I'm obviously using the `stlink` server backend for `cortex-debug`, and I have tried using CubeIDE to get the exact gdb-server arguments used when it launches a debug session.  However even when I do that, I still end up with a corrupted stack pointer or missing sources?   The symptom is that the debug session says something to the effect of "??@<hex>  Unknown Source".  It also seems to have problems halting the core at startup.

Here's something representative of the config I'm using right now:

 

 

{
 "version": "0.2.0",
 "configurations": [
 {
 "cwd": "${workspaceFolder}",
 "executable": "${workspaceFolder}/FSBL/build/<my_project_name>.elf",
 "name": "Debug with ST-Link",
 "request": "launch",
 "type": "cortex-debug",
 "runToEntryPoint": "main",
 "showDevDebugOutput": "none",
 "servertype": "stlink",
 "serverArgs": [
 "-l", "1", "-s", "-m", "1", "-k",
 ],
 },
 ]
}

 

I've tried using a lot more arguments spelling out all the possible source locations, post-launch commands, etc, but so far it's been to no avail. Any help is appreciated!

 

This topic has been closed for replies.
Best answer by alister

https://github.com/Marus/cortex-debug/issues/1104 lists a working VS Code launch.json (debug configuration) and includes a plausible STM32N6-specific explanation for it.

7 replies

ST Employee
February 11, 2025

Hello @JNT

This issue is spotted and under investigation for STM32N6 product, the launch.json file is created with default STLink configuration  (Not specific to N6), so not able to start a debug session (Internal ticket number: 197953), I will keep you updated! 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
alister
alisterBest answer
Senior III
April 9, 2025

https://github.com/Marus/cortex-debug/issues/1104 lists a working VS Code launch.json (debug configuration) and includes a plausible STM32N6-specific explanation for it.

Associate
February 27, 2025

@JNT  were you able to resolve this issue? I am struggling with the same issue currently, I cannot debug a program using the VSCode plugin.

 

Additionally, there seems to be no way to debug a non-secure application in STM32CubeIDE, have you encountered that issue as well?

JNTAuthor
Associate
March 10, 2025

I haven't tried debugging a non-secure application yet, and I still haven't solved the debugging in VSCode problem unfortunately.  Hoping ST sorts this out so that we can actually get some real work in on this platform.  At the moment there are a lot of rough edges (RIF is another bane of my existence right now).

Explorer II
March 29, 2025

I'm also unable to build and run for the STM32N6 Discovery board (STM32N6570-DK) with VSCode.

The VSCode extension creates two launch.json profiles, which do not work for me:

  • Build & Debug Microcontroller - ST-Link
  • Attach to Microcontroller - ST-Link

Given some of the comments above, it seemed possible the VSCode extension was not updated for the STM32N6 board.

Unfortunately, I cannot find the source code for that extension to verify this.In an attempt to workaround this, I inspected the launch.json for STM32H5. This module uses TrustZone and generates the 6 launch.json profiles as expected:

  1. Build & Debug Secure Microcontroller - ST-Link
  2. Attach to Secure Microcontroller - ST-Link
  3. Build & Debug NonSecure Microcontroller - ST-Link
  4. Attach to NonSecure Microcontroller - ST-Link
  5. Build & Debug Microcontroller Secure and NonSecure - ST-Link
  6. Attach to Secure and NonSecure Microcontroller - ST-Link

I modified VSCode launch.json + tasks.json to match the STM32H5 example, updating module references to STM32N6 as needed. I had to replace all "${command:STM32VSCodeExtension.trustZoneNonSecureTarget}" references in these files as VSCode extension was not populating these. Again, without extension source code access this is difficult to debug so I hardcoded for now.

This made some "progress", however I now see an error upon flashing:

* Executing task: STM32_Programmer_CLI --connect port=swd --download /Users/bradylaw/code/bitcam-bringup/bitcam/AppliNonSecure/build/bitcam_AppliNonSecure.elf -hardRst -rst --start

-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------

ST-LINK SN : 003800393333511831363730
ST-LINK FW : V3J16M7
Board : STM32N6570-DK
Voltage : 3.27V
SWD freq : 8000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x486
Revision ID : Rev B
Device name : STM32N6xx
Device type : MCU
Device CPU : Cortex-M55
BL Version : --

Opening and parsing file: bitcam_AppliNonSecure.elf


Memory Programming ...
File : bitcam_AppliNonSecure.elf
Size : 3.01 KB
Address : 0x24100000



Erasing memory corresponding to sector 0:
Download in Progress:
[==================================================] 100%

File download complete
Time elapsed during download operation: 00:00:00.006

Hard reset is performed

MCU Reset
Error: Unable to run MCU!
Error: Error code: 32

 The screen goes black but there is some kind of issue during the flashing step. Perhaps related to the FSBL with STM32N6 but I need to read up on that more.

Could you point us towards the documented way to flash the discovery board using STM32_Programmer_CLI?

Explorer II
March 29, 2025

Looking a bit closer, perhaps bootstrapping a project using STM32CubeN6 instead of STM32CubeMX is the way to go right now. It seems there are a lot of discovery kit specific instructions.

https://github.com/STMicroelectronics/STM32CubeN6/blob/main/Projects/STM32N6570-DK/Templates/Template/README.md#how-to-use-it-

https://www.st.com/resource/en/user_manual/um3249-getting-started-with-stm32cuben6-for-stm32n6-series-stmicroelectronics.pdf 

There are probably ways to adapt those README instructions to some VSCode launch.json+tasks.json configuration, but those will depend upon the template you select.

ST Employee
May 6, 2025

Hello everyone, 

It should work with the port selection to access port 1 on N6

Please add this line in your launch.json "serverApID": "1" in your stlink section.

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.