Skip to main content
Associate II
Dec 13, 2024 11:05 PM UTC
Solved

No boot after flashing the STM32MP157f-dk2 SD card

Hi all,


I just got the board and off course now want to follow the official page (https://wiki.stmicroelectronics.cn/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP135x-DK/Let%27s_start/Populate_the_target_and_boot_the_image) for flashing.

OS windows 10.

STMCubeProgrammer v2.18.0

  1. inserted SD card to board, SW1 set to USB, connected PC with CN7
  2. started the STMCubeProgrammer and successfully connected to USB1 (so drivers OK)
  3. downloaded en.FLASH-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v24.11.06.tar.gz and unpacked
  4. run in cmd: C:\Program Files(x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=usb1 -w C:\<path>\FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv
  5. see result Download.png (as I never saw a correct log I think here something went wrong after "Reconnecting the device ...")
  6. on display: "DFU alt info setting: done"
    "crq->brequest: 0x0"
  7. power off, SW1 set to SD card (position oppostite from USB), power ON
  8. nothing on display and on uart

Regards

This topic has been closed for replies.
anpaBest answer
Associate II
Dec 22, 2024 10:23 AM UTC

HI PatrickF,

 

Good news, I found a way to download.

  • I run again start "STM32 USB DFU DRIVER" pnputil -i -a %0\..\Driver\STM32Bootloader.inf but without connected USB and I got a message success (but not sure was this step actual needed).
  • Open CubeProgrammer.
  • So first attempt is like I described and crashes the programmer The usb state is Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000.
  • Than without resetting the board I reopen the programmer connect the board but than it is reported Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z so I thought it will work, but crashes again.
  • Luckily the 3 attempt works until the end and downloads ALL (important dont reset the board leave the state from 2nd attempt)

 

anpa_0-1734862733335.png

Attached the uart log with all 3 attempts.

This issue is resolved!!!!

Regards & thx for support,

anpa

 

 

11 replies

PatrickF
ST Employee
Dec 16, 2024 1:39 PM UTC

Hi,

this is two  common pitfalls which could make this to happen:

  1. Supply is detected as non-compliant with Type-C power supply. Red led bright and there is message on the board console log (STLINK USB Virtual Com Port).
  2. When using Linux over a Virtual Machine, when downloaded uBoot starts, the USB port newly enumerated should be defined to connect automatically to the virtual machine (as usually by default connected to Windows OS).

Regards,

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
anpaAuthor
Associate II
Dec 16, 2024 6:00 PM UTC

Hi PatrickF,

 

I use official Raspi 4 (ouput 5.1V 3A 15.3W) charger which should be ok for the board. 

I use windows 10 pure and no VM or wsl2. I dont see any error anywhere.

I suspect 3 things.

  • Something wrong with usb port on board but than it partially downloaded  as seen on the picture I attached.
  • I suspect some bug in the Cube programmer as it basically crashes after message "reconnecting devices"
  • some problem with the usb on my laptop (but I doubt this)

I flashed so far the booloader with balenaEtcher to the SDCard and this is ok I reach the u-boot.

I also did this https://bootlin.com/blog/building-a-linux-system-for-the-stm32mp1-basic-system/ and works perfectly.

So my problem is CubeProgrammer is not transferring files to the SDCard. Strange thing is why the programmer crashes and not displaying some error code? Should I try some older versions and/or install a VM and flash it from linux?

Regards,

Andor

 

PatrickF
ST Employee
Dec 17, 2024 8:58 AM UTC

ok, so maybe a missing USB driver on the PC (I guess during CubeProg install).
Could you look at Windows Device Manager (after the 'reconnect') to see if 'reconnected' DFU is present.like this

PatrickF_0-1734425817623.png

 

Regards,

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
anpaAuthor
Associate II
Dec 19, 2024 8:53 AM UTC

Hi PatricF,

I tried to reinstall all again but no luck.

I debugged the STM32Bootloader.bat and from if else it enters the:

start "STM32 USB DFU DRIVER" pnputil -i -a %0\..\Driver\STM32Bootloader.inf

but the log I get:

 

pnputil -i -a "c:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\Drivers\DFU_Driver\Driver\STM32Bootloader.inf"
Microsoft PnP Utility

Processing inf : STM32Bootloader.inf
Failed to install the driver : No more data is available.


Total attempted: 1
Number successfully imported: 0

 

regards

PatrickF
ST Employee
Dec 19, 2024 10:07 AM UTC

Hi @anpa 

strange as CubeProgramer should have been installed in C:\Program Files and not c:\Program Files (x86)

What result did you get if you right click on STM32Bootloader.inf file then select install ?

Regards.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
anpaAuthor
Associate II
Dec 19, 2024 10:23 AM UTC

Hi,

 

anpa_0-1734603799481.png

Regards

anpaAuthorBest answer
Associate II
Dec 22, 2024 10:23 AM UTC

HI PatrickF,

 

Good news, I found a way to download.

  • I run again start "STM32 USB DFU DRIVER" pnputil -i -a %0\..\Driver\STM32Bootloader.inf but without connected USB and I got a message success (but not sure was this step actual needed).
  • Open CubeProgrammer.
  • So first attempt is like I described and crashes the programmer The usb state is Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000.
  • Than without resetting the board I reopen the programmer connect the board but than it is reported Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z so I thought it will work, but crashes again.
  • Luckily the 3 attempt works until the end and downloads ALL (important dont reset the board leave the state from 2nd attempt)

 

anpa_0-1734862733335.png

Attached the uart log with all 3 attempts.

This issue is resolved!!!!

Regards & thx for support,

anpa