Skip to main content
PGE
Associate III
July 23, 2020
Solved

How to enable 3 USB ports on STM32MP1

  • July 23, 2020
  • 6 replies
  • 3885 views

According to different STM32MP1 documentation such as STM32MP1-Peripheral-USB_Host_interface_USBH or STM32MP1-Peripheral-USB-On-The-Go-Full-and-HighSpeed-interface presentation there is two USB phy, one dual port HS phy and one single port FS phy.

In my understanding I should be able to enable 3 USB host port, two HS and one FS.

I am using the STM32CubeMX tool but I am unable to enable such 3 ports. I am able to enable two HS port but I am unable to enable OTG port. If I disable one HS port I am able to enable OTG port. So it seems STM32CubeMX allows to enable only two ports at the same time.

 

Is this an issue of STM32CubeMX or it's a real limitation of the chip ?

Note, I have tried with different package with the same results

 

Many thanks in advance for any help

This topic has been closed for replies.
Best answer by PatrickF

Hello,

This is a limitation in CubeMX, I confirm you could really use three host ports (2 x high-speed + 1 x full-speed).

You have to edit the device tree manually for this case. see https://wiki.st.com/stm32mpu/wiki/OTG_device_tree_configuration#DT_configuration_example_as_full-speed_OTG-2C_with_micro-B_connector

Notice that OTG host HW/driver has some limitations which make it not recommended to be connected to an USB Hub.

6 replies

PatrickF
PatrickFBest answer
ST Employee
July 23, 2020

Hello,

This is a limitation in CubeMX, I confirm you could really use three host ports (2 x high-speed + 1 x full-speed).

You have to edit the device tree manually for this case. see https://wiki.st.com/stm32mpu/wiki/OTG_device_tree_configuration#DT_configuration_example_as_full-speed_OTG-2C_with_micro-B_connector

Notice that OTG host HW/driver has some limitations which make it not recommended to be connected to an USB Hub.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
Visitor II
May 16, 2024

Hi,

I had a similar problem with kernel 6.1.28, but I managed to solve it.I now can use all three USB ports ( 2xHS + OTG_FS )

I had the following message when connecting the board in peripheral mode :

dwc2 49000000.usb-otg: Failed to exit L1 sleep state in 200us

Patch : https://lore.kernel.org/lkml/20201123090114.12641-4-amelie.delaunay@st.com/

 

From: Amelie Delaunay <amelie.delaunay@st.com>
To: Minas Harutyunyan <hminas@synopsys.com>,
	Felipe Balbi <balbi@kernel.org>,
	Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Cc: <linux-usb@vger.kernel.org>, <linux-kernel@vger.kernel.org>,
	<linux-stm32@st-md-mailman.stormreply.com>,
	Fabrice Gasnier <fabrice.gasnier@st.com>,
	Amelie Delaunay <amelie.delaunay@st.com>
Subject: [PATCH 3/3] usb: dwc2: disable Link Power Management on STM32MP15 HS OTG
Date: Mon, 23 Nov 2020 10:01:14 +0100	[thread overview]
Message-ID: <20201123090114.12641-4-amelie.delaunay@st.com> (raw)
In-Reply-To: <20201123090114.12641-1-amelie.delaunay@st.com>

Link Power Management (LPM) on STM32MP15 OTG HS encounters instabilities
with some Host controllers. OTG core fails to exit L1 state in 200us:
"dwc2 49000000.usb-otg: Failed to exit L1 sleep state in 200us."
Then the device is still not enumerated.

To avoid this issue, disable Link Power Management on STM32MP15 HS OTG.

Signed-off-by: Amelie Delaunay <amelie.delaunay@st.com>
---
 drivers/usb/dwc2/params.c | 4 ++++
 1 file changed, 4 insertions(+)

diff --git a/drivers/usb/dwc2/params.c b/drivers/usb/dwc2/params.c
index 9e5dd7f3f2f6..92df3d620f7d 100644
--- a/drivers/usb/dwc2/params.c
+++ b/drivers/usb/dwc2/params.c
@@ -194,6 +194,10 @@ static void dwc2_set_stm32mp15_hsotg_params(struct dwc2_hsotg *hsotg)
 	p->host_perio_tx_fifo_size = 256;
 	p->ahbcfg = GAHBCFG_HBSTLEN_INCR16 << GAHBCFG_HBSTLEN_SHIFT;
 	p->power_down = DWC2_POWER_DOWN_PARAM_NONE;
+	p->lpm = false;
+	p->lpm_clock_gating = false;
+	p->besl = false;
+	p->hird_threshold_en = false;
 }
 
 const struct of_device_id dwc2_of_match_table[] = {
-- 
2.17.1

 

Here is a working device-tree allowing to use both USB in high-speed and OTG as full-speed:

 

/dts-v1/;

#include "stm32mp157c-odyssey-som.dtsi"

/ {
	model = "Seeed Studio Odyssey-STM32MP157C Board";
	compatible = "seeed,stm32mp157c-odyssey",
		 "seeed,stm32mp157c-odyssey-som", "st,stm32mp157";

	aliases {
		ethernet0 = &ethernet0;
		serial0 = &uart4;
	};

	chosen {
		stdout-path = "serial0:115200n8";
	};
};

&dcmi {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&dcmi_pins_b>;
	pinctrl-1 = <&dcmi_sleep_pins_b>;
};

&ethernet0 {
	status = "okay";
	pinctrl-0 = <&ethernet0_rgmii_pins_a>;
	pinctrl-1 = <&ethernet0_rgmii_sleep_pins_a>;
	pinctrl-names = "default", "sleep";
	phy-mode = "rgmii-id";
	max-speed = <1000>;
	phy-handle = <&phy0>;
	assigned-clocks = <&rcc ETHCK_K>, <&rcc PLL4_P>;
	assigned-clock-parents = <&rcc PLL4_P>;
	assigned-clock-rates = <125000000>; /* Clock PLL4 to 750Mhz in ATF/U-Boot */
	st,eth-clk-sel;

	mdio0 {
		#address-cells = <1>;
		#size-cells = <0>;
		compatible = "snps,dwmac-mdio";
		phy0: ethernet-phy@7 { /* KSZ9031RN */
			reg = <7>;
			reset-gpios = <&gpiog 0 GPIO_ACTIVE_LOW>; /* ETH_RST# */
			reset-assert-us = <10000>;
			reset-deassert-us = <300>;
		};
	};
};

&i2c1 {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&i2c1_pins_a>;
	pinctrl-1 = <&i2c1_sleep_pins_a>;
	i2c-scl-rising-time-ns = <100>;
	i2c-scl-falling-time-ns = <7>;
	status = "okay";
	/delete-property/dmas;
	/delete-property/dma-names;
};

&sdmmc1 {
	pinctrl-names = "default", "opendrain", "sleep";
	pinctrl-0 = <&sdmmc1_b4_pins_a>;
	pinctrl-1 = <&sdmmc1_b4_od_pins_a>;
	pinctrl-2 = <&sdmmc1_b4_sleep_pins_a>;
	cd-gpios = <&gpioi 3 (GPIO_ACTIVE_LOW | GPIO_PULL_UP)>;
	disable-wp;
	st,neg-edge;
	bus-width = <4>;
	vmmc-supply = <&v3v3>;
	status = "okay";
};

&uart4 {
	pinctrl-names = "default";
	pinctrl-0 = <&uart4_pins_a>;
	/delete-property/dmas;
	/delete-property/dma-names;
	status = "okay";
};

&usbotg_hs {
	compatible = "st,stm32mp15-fsotg", "snps,dwc2";
	pinctrl-names = "default";
	pinctrl-0 = <&usbotg_fs_dp_dm_pins_a>;
	dr_mode = "device";
	status = "okay";
};

&pinctrl {
	usbotg_hs_pins_b: usbotg-hs-1 {
		pins {
			pinmux = <STM32_PINMUX('G', 12, ANALOG)>; /* OTG_ID */
		};
	};
};

&usbphyc {
	status = "okay";
};


&usbphyc_port0 {
	st,tune-hs-dc-level = <2>;
	st,enable-fs-rftime-tuning;
	st,enable-hs-rftime-reduction;
	st,trim-hs-current = <15>;
	st,trim-hs-impedance = <1>;
	st,tune-squelch-level = <3>;
	st,tune-hs-rx-offset = <2>;
	st,no-lsfs-sc;
	connector {
		compatible = "usb-a-connector";
		vbus-supply = <&vbus_sw>;
	};
};


&usbphyc_port1 {
	st,tune-hs-dc-level = <2>;
	st,enable-fs-rftime-tuning;
	st,enable-hs-rftime-reduction;
	st,trim-hs-current = <15>;
	st,trim-hs-impedance = <1>;
	st,tune-squelch-level = <3>;
	st,tune-hs-rx-offset = <2>;
	st,no-lsfs-sc;
	connector {
		compatible = "usb-a-connector";
		vbus-supply = <&vbus_sw>;
	};
};

&vdd_usb {
	regulator-always-on;
};

&vdda {
	regulator-always-on;
};

&usbh_ohci {
	phys = <&usbphyc_port0> ;
	phy-names="usb2-phy";
	status = "disabled";
};

&usbh_ehci{
	phys = <&usbphyc_port0>, <&usbphyc_port1 1>;
	status = "okay";
};

 

 

PGE
PGEAuthor
Associate III
July 24, 2020

Ok many thanks for your clear reply

Any other known limitation ? Is there any documentation with all known limitation / issue ?

PatrickF
ST Employee
July 24, 2020
In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
PGE
PGEAuthor
Associate III
September 3, 2020

@PatrickF​ According to your link above default IOs for USB OTG in full-speed mode are PA11 and PA12. These are general purpose IOs, are they powered by VDD or VDD_USB ? As USB is 3.3V signals does-it work well also with 1.8V VDD powered STM32MP157 ?

Thanks in advance for clarification

PatrickF
ST Employee
September 3, 2020

PA11 and PA12 are specific IOs and supplied by VDD_USB (3.3V typ.) when used as OTG_FS data pins, VDD otherwise.

No issue regarding VDD=1.8V

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent