2020-07-27 6:21 AM
I'm trying to make FreeRTOS application which is involving ADC and sending messages via virtual UART to Cortex A7. So I began with example called OpenAMP_FreeRTOS_echo in the cube fw version 1.2.0. That example worked good. I saw echo on /dev/ttyRPMSG0. Then I tried to incorporate ADC into that code but without success (I made succes with ADC + virtual UART without using FreeRTOS, but I want to make FreeRTOS working). I had a lot of trouble using System Workbench in terms of ST-Link detection (I always had to change COM port in the Debug Configuration) and I read on this forum that there were troubles in using FreeRTOS and those troubles are solved in Cube IDE 1.2.1.
https://community.st.com/s/question/0D50X0000BI0vctSQB/freertos-does-not-run-on-stm32mp1-m4-core
So I recently switched to Cube IDE v1.4.0, but there I have trouble on stopping on breakpoint. I placed break point on lines after main which must be executed (i.e. HAL_Init), but the debug is not stopped.
Thanks in advance for the answer,
Nenad
Solved! Go to Solution.
2020-07-27 6:29 AM
Hi @NGajic
In production mode, where M4 code is launched by A7, there is a delay between M4 core start and debugger attachment.
So all breakpoint set "too early" in the code are ignored.
Please confirm you can set breakpoint further in your code.
Usual tips to w/a this is either to add a sleep of few seconds at beginning of your main, or create while loop you can then bypass with debugger afterward.
Olivier
2020-07-27 6:29 AM
Hi @NGajic
In production mode, where M4 code is launched by A7, there is a delay between M4 core start and debugger attachment.
So all breakpoint set "too early" in the code are ignored.
Please confirm you can set breakpoint further in your code.
Usual tips to w/a this is either to add a sleep of few seconds at beginning of your main, or create while loop you can then bypass with debugger afterward.
Olivier
2020-07-27 6:37 AM
Hi OlivierG(iroud), :)
Thanx for your fast answer. Yeah, debugger stops after some time and I guessed that there is something in debugger. I will add delay.
Nenad