Question
What is the cause of the error that occurs when loading the Cortex-M4 FW to the Cortex-A7 (Linux)?
- December 16, 2020
- 2 replies
- 4261 views
We have confirmed the operation on our original board that
"STM32MP151CAA3" mounted on.
When I start our Cortex-A7 (Linux) FW and try to load our Cortex-M4 (RTOS: uC3) FW , an error message is output on the console of Linux.
The steps when an error occurs is described below.
Is there any possible cause for the error?
--Steps--
1) Write our Cortex-A7 (Linux) FW to a SD card and start it with our original board.
2) Build our Cortex-M4 (RTOS: uC3) FW. ⇒ Build is successful.
3) Transfer our Cortex-M4 (RTOS: uC3) FW to our original board by scp.
4) Start our Cortex-M4 (RTOS: uC3) FW by Cortex-A7 (Linux) FW.
⇒ Linux console shows the error message.
Best Regards,
H. Masuda