Skip to main content
Kim.Andy
Associate II
March 2, 2020
Question

UART4 RX Signal level

  • March 2, 2020
  • 2 replies
  • 3532 views

I use the UART4 like the following initialization.

void uart4_configuration(void)
{
 GPIO_InitTypeDef GPIO_InitStructure;
 USART_InitTypeDef USART_InitStructure;
 /* enable usart clock */
 RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE);
 
 
 RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
 
 
 // Configure USART Tx as alternate function
 GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; //GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
 GPIO_InitStructure.GPIO_Pin = RS485AXM_TX_PIN;
 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
 GPIO_Init(RS485AXM_COM_PORT, &GPIO_InitStructure);
 
 // Configure USART Rx as alternate function
 GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN; //GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
 GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
 GPIO_InitStructure.GPIO_Pin = RS485AXM_RX_PIN;
 GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
 GPIO_Init(RS485AXM_COM_PORT, &GPIO_InitStructure);
 
 GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_UART4);
 GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_UART4);
 
 
 USART_StructInit(&USART_InitStructure);
 USART_InitStructure.USART_BaudRate = 9600;
 USART_Init(UART4, &USART_InitStructure);
 
 USART_Cmd(UART4, ENABLE);
 
 NVIC_EnableIRQ(UART4_IRQn);
}

The Rx signal level is abnormal like the following.

0690X00000DYODdQAP.jpg

The low level is not the zero(ground) level.

But the Tx level is ok like the followings.

0690X00000DYODiQAP.jpg

Although I detach the RX Pin from the PCB Board, and tie with the TX Pin,

RX/TX Pin level is like the abnormal level(the first image)

Is the initialization is wrong?

Thanks

This topic has been closed for replies.

2 replies

Olivier GALLIEN
ST Technical Moderator
March 2, 2020

Hi @AK.12.26im​ 

In order to reach faster the relevant community could you please add further information about your context ?

chip, board, application ...

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee
March 2, 2020

Sound like your usage of GPIO_Init() is wrong, you miss the GPIO_InitStruct.Alternate setting and GPIO_PinAFConfig() does not exist in CubeMP1 drivers.

Here is an example of UART AF mux setting generated by CubeMx:

 /**UART4 GPIO Configuration 
 PD1 ------> UART4_TX
 PH14 ------> UART4_RX 
 */
 GPIO_InitStruct.Pin = GPIO_PIN_1;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF8_UART4;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
 
 GPIO_InitStruct.Pin = GPIO_PIN_14;
 GPIO_InitStruct.Mode = GPIO_MODE_AF;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Alternate = GPIO_AF8_UART4;
 HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent