cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MPU ecosystem release V3.1.0 release is online !

Olivier GALLIEN
ST Employee

Dear STM32 MPU Community,

We are please to announce that New MP1 Ecosystem V3.1.0 is available.

It contains :

  • Openstlinux-5.10-dunfell-mp1-21-11-17
  • STM32MP1Cube V1.5.0
  • STM32CubeIDE V1.8.0
  • STM32CubeMX V6.4
  • STM32CubeProgrammer V2.9.0

Please check out the STM32MP15 ecosystem release note - stm32mpu on STM32 Wiki to get complete description of content and new features.

*** Main NEW features of the STM32MP15-ecosystem-v3.1.0 release ***

  • Coprocessor firmware Authentication support
  • QSPI NAND performance improvements
  • Linux KGDB support
  • DMA pause & resume support
  • stm32key command update for easy evaluation of STM32MP15 secure boot
  • Enabling LPDDR2 / LPDDR3 PHY built-in Read Valid training (RVTRN)

*** 1st Buildroot distribution based on ST Linux BSP and supported by Bootlin !! ***

Read STM32MP15 Buildroot release note - v3.1.0

Wiki for previous ecosystem are still available :

Ecosystem-V2-Wiki

Ecosystem-V1-Wiki

Hope you will enjoy this new release.

In case any questions, issues .. this Community is made for you !

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0