cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157AAA3 only support 16bit-LPDDR3?

Mokail
Associate II

I used 1GB LPDDR3 at STM32MP157AAA3 chips.but it's only read 512MB:sad_but_relieved_face:

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
PatrickF
ST Employee

Maybe double check your CubeMX and effective DT settings.

You should have somewhere: #define DDR_MEM_SIZE 0x40000000 and relevant DDR controller settings

Find below an example of a possible LPDDR3 setting.

// SPDX-License-Identifier: GPL-2.0+ OR BSD-3-Clause

/*

 * Copyright (C) 2018, STMicroelectronics - All Rights Reserved

 *

 * 8Gb LPDDR3 32-bit BGA / SDP / 533 Mhz

 * Reference used H9CCNNNBGALAR-NXD

 *

 * DDR type / Platform   LPDDR3

 * freq      533MHz

 * width   32

 * datasheet   0

 * DDR density   8

 * timing mode   optimized

 * Scheduling/QoS options : type = 2

 * address mapping : RBC

 * Tc > + 85C : N

 */

#define DDR_MEM_NAME "LPDDR3 8Gb 533MHz v1.45"

#define DDR_MEM_SPEED 533000

#define DDR_MEM_SIZE 0x40000000

#define DDR_MSTR 0x00040008

#define DDR_MRCTRL0 0x00000010

#define DDR_MRCTRL1 0x00000000

#define DDR_DERATEEN 0x00000001

#define DDR_DERATEINT 0x00800000

#define DDR_PWRCTL 0x00000000

#define DDR_PWRTMG 0x00400010

#define DDR_HWLPCTL 0x00000000

#define DDR_RFSHCTL0 0x00210000

#define DDR_RFSHCTL3 0x00000000

#define DDR_RFSHTMG 0x00400070

#define DDR_CRCPARCTL0 0x00000000

#define DDR_DRAMTMG0 0x111B1217

#define DDR_DRAMTMG1 0x00040423

#define DDR_DRAMTMG2 0x04080C0F

#define DDR_DRAMTMG3 0x00A0A00C

#define DDR_DRAMTMG4 0x0804060C

#define DDR_DRAMTMG5 0x02020808

#define DDR_DRAMTMG6 0x02020006

#define DDR_DRAMTMG7 0x00000202

#define DDR_DRAMTMG8 0x00004405

#define DDR_DRAMTMG14 0x00000076

#define DDR_ZQCTL0 0xC2000040

#define DDR_DFITMG0 0x02060104

#define DDR_DFITMG1 0x00000202

#define DDR_DFILPCFG0 0x07000000

#define DDR_DFIUPD0 0xC0400003

#define DDR_DFIUPD1 0x00000000

#define DDR_DFIUPD2 0x00000000

#define DDR_DFIPHYMSTR 0x00000001

#define DDR_ADDRMAP1 0x00080808

#define DDR_ADDRMAP2 0x00000000

#define DDR_ADDRMAP3 0x00000000

#define DDR_ADDRMAP4 0x00001F1F

#define DDR_ADDRMAP5 0x07070707

#define DDR_ADDRMAP6 0x0F070707

#define DDR_ADDRMAP9 0x00000000

#define DDR_ADDRMAP10 0x00000000

#define DDR_ADDRMAP11 0x00000000

#define DDR_ODTCFG 0x04000400

#define DDR_ODTMAP 0x00000000

#define DDR_SCHED 0x00000C01

#define DDR_SCHED1 0x00000000

#define DDR_PERFHPR1 0x01000001

#define DDR_PERFLPR1 0x08000200

#define DDR_PERFWR1 0x08000400

#define DDR_DBG0 0x00000000

#define DDR_DBG1 0x00000000

#define DDR_DBGCMD 0x00000000

#define DDR_POISONCFG 0x00000000

#define DDR_PCCFG 0x00000010

#define DDR_PCFGR_0 0x00010000

#define DDR_PCFGW_0 0x00000000

#define DDR_PCFGQOS0_0 0x02100C03

#define DDR_PCFGQOS1_0 0x00800100

#define DDR_PCFGWQOS0_0 0x01100C03

#define DDR_PCFGWQOS1_0 0x01000200

#define DDR_PCFGR_1 0x00010000

#define DDR_PCFGW_1 0x00000000

#define DDR_PCFGQOS0_1 0x02100C03

#define DDR_PCFGQOS1_1 0x00800040

#define DDR_PCFGWQOS0_1 0x01100C03

#define DDR_PCFGWQOS1_1 0x01000200

#define DDR_PGCR 0x01442E02

#define DDR_PTR0 0x0022AA5B

#define DDR_PTR1 0x01B1A068

#define DDR_PTR2 0x042A16E7

#define DDR_ACIOCR 0x38400812

#define DDR_DXCCR 0x00000910

#define DDR_DSGCR 0x9100025F

#define DDR_DCR 0x0000000D

#define DDR_DTPR0 0x46D78BD0

#define DDR_DTPR1 0x117000D8

#define DDR_DTPR2 0x00041076

#define DDR_MR0 0x00000000

#define DDR_MR1 0x000000C3

#define DDR_MR2 0x00000006

#define DDR_MR3 0x00000003

#define DDR_ODTCR 0x00000000

#define DDR_ZQ0CR1 0x00000018

#define DDR_DX0GCR 0x0000C881

#define DDR_DX0DLLCR 0x40000000

#define DDR_DX0DQTR 0xFFFFFFFF

#define DDR_DX0DQSTR 0x3DB02000

#define DDR_DX1GCR 0x0000C881

#define DDR_DX1DLLCR 0x40000000

#define DDR_DX1DQTR 0xFFFFFFFF

#define DDR_DX1DQSTR 0x3DB02000

#define DDR_DX2GCR 0x0000C881

#define DDR_DX2DLLCR 0x40000000

#define DDR_DX2DQTR 0xFFFFFFFF

#define DDR_DX2DQSTR 0x3DB02000

#define DDR_DX3GCR 0x0000C881

#define DDR_DX3DLLCR 0x40000000

#define DDR_DX3DQTR 0xFFFFFFFF

#define DDR_DX3DQSTR 0x3DB02000

#include "stm32mp15-ddr.dtsi"

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Mokail
Associate II

Can you see me another problem?i used sii9022 chip for hdmi,but it's not work ​and always busy.:sad_but_relieved_face: